This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:pluto:hacking:listening_to_yourself [11 Jul 2019 01:41] – [Conclusion] Robin Getz | university:tools:pluto:hacking:listening_to_yourself [05 Aug 2019 23:06] (current) – [Tx On, and not sending a signal] Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Self Reception on the ADALM-PLUTO ====== | ====== Self Reception on the ADALM-PLUTO ====== | ||
- | Everyone has sung to a song on the radio, and it sounds great, as long as the radio is loud enough to drown out your terrible voice (or is that just me?). This is a phenomena | + | Everyone has sung to a song on the radio, and it sounds great, as long as the radio is loud enough to drown out your terrible voice (or is that just me?). This is a phenomenon |
- | The ADALM-PLUTO can do this to if you are not careful. The device will have Tx LO Leakage, and the receiver will pick that up, and may swamp out the signal you desire to actually receive. | + | The ADALM-PLUTO can do this too if you are not careful. The device will have Tx LO Leakage, and the receiver will pick that up and may swamp out the signal you desire to actually receive. |
===== Tx On, and sending a signal ===== | ===== Tx On, and sending a signal ===== | ||
Line 11: | Line 11: | ||
{{ : | {{ : | ||
- | This shows the peak at the signal (at 2405 MHz, where we expect it), and a LO leakage at 2402 MHz. It's difficult to see what this really means in terms of signal power, so we can look at the actual gain is set to by the Automatic Gain Control (ACG), and the Receive Signal Strength Indicator (RSSI). | + | This shows the peak at the signal (at 2405 MHz, where we expect it), and a LO leakage at 2402 MHz. It's difficult to see what this really means in terms of signal power, so we can look at the actual gain is set to by the Automatic Gain Control (AGC), and the Receive Signal Strength Indicator (RSSI). |
{{ : | {{ : | ||
Line 25: | Line 25: | ||
{{ : | {{ : | ||
- | Now our RSSI has gone to 90.5 dB and the hardware gain is set to 68 dB (which is still not at the max gain of the device), we are listening to ourselves, not the actual RF. | + | Now our RSSI has gone to 90.5 dB and the hardware gain is set to 68 dB (which is still not at the max gain of the device), we are listening to our own LO leakage, not the actual RF signal. |
===== Tx Off ===== | ===== Tx Off ===== | ||
Line 36: | Line 36: | ||
dev ' | dev ' | ||
</ | </ | ||
+ | |||
+ | This is the equivalent C source of: | ||
+ | < | ||
+ | /* Create IIO Context */ | ||
+ | ctx = iio_create_context_from_uri(" | ||
+ | |||
+ | /* Find IIO device in current context */ | ||
+ | dev = iio_context_find_device(ctx, | ||
+ | |||
+ | /* Find the IIO output channel in the current device */ | ||
+ | ch = iio_device_find_channel(dev, | ||
+ | |||
+ | /* Write a one into the IIO channel attribute */ | ||
+ | ret = iio_channel_attr_write_longlong(dev, | ||
+ | </ | ||
Then we get: | Then we get: | ||
Line 41: | Line 56: | ||
{{ : | {{ : | ||
{{ : | {{ : | ||
+ | |||
+ | ===== Tx On, but offset more than your channel ===== | ||
+ | |||
+ | If we shift things around a bit - if we configure things for an LTE10 signal, (LTE10 filter, with an LTE10 signal going out the DAC at full scale), and set the Tx and Rx to the same (2400 MHz), we can see this: | ||
+ | |||
+ | {{ : | ||
+ | {{ : | ||
+ | |||
+ | By offsetting things in 10 MHz steps, how far do things need to be away, so that it stops affecting the receiver: | ||
+ | |||
+ | ^ offset | ||
+ | | RSSI | 48.50 dB | 86.75 dB | 105.00 dB | 112.75 dB | 116.75 dB | 117.00 dB | 117.5 dB | | ||
+ | | ACG Gain | 25 dB | 32 dB | 59 dB | 62 dB | 67 dB | 69 dB | 71 dB | | ||
+ | |||
+ | This doesn' | ||
===== Conclusion ===== | ===== Conclusion ===== |