This is an old revision of the document!
ADALM-PLUTO Hardware
Whether you want to understand the changes between revisions, or just understand how to probe the PCB, this is where all the information should be.
Connectors
The PlutoSDR includes a button (S1
on the PCB), and two USB connectors.
The button can be defined by software, it is normally held on with a paper clip or thumb tack during power on to put the device into a recovery mode. It can be re-purposed to do other things.
The first USB connector (the middle one) is the USB OTG connector (can be the USB HOST connector (cabled to a USB peripheral), or the USB peripheral connector (cabled to a USB Host)).
The second USB connector (the one on the side) is for power only when running in Host mode.
Removing the case
The plastic case comes off quite easily, with the removal of two black Phillips screws on the bottom of the case. This is a picture of the pre-production Rev B boards. The production version may be different. It will for sure be CE and FCC certified. (already passed).
Removing the screws will allow you to take the top off the case, and expose the PCB.
If you want to remove the PCB, and place it on the table, we recommend that you attach Cylindrical Bumpers (also known as feet), on the PCB to protect the components on the bottom of the PCB. These are not included in the design, and must be purchased separately (as we don't expect too many people wanting to do this).
Revisions
Different revisions of the PlutoSDR does not include any major functionality changes, and there is no difference for end users (there may be minor internal feature changes). While it is natural to want the “latest” version, there is no specified functionality changes. All revisions are:
1x Rx SMA, Tuning from 325
MHz to 3.8
GHz, 200
kHz - 20
MHz of instantaneous bandwidth
1x Tx SMA, Tuning from 325
MHz to 3.8
GHz, 200
kHz - 20
MHz of instantaneous bandwidth
-
-
Linux / libIIO based software stack, compatible with MATLAB, Simulink,
GNU Radio, Python, and others.
When you order from ADI's authorized channels, you may get any revision listed below; there is no way to order one specific revision (it's a single part number), so do not ask - it's not possible. Normally inventory is managed via a FIFO (First In; First Out) mechanism, so the oldest inventory is shipped when an order is placed. However - warehouses have been known to misplace a box, and ship older inventory later.
If you really want to purchase a specific version - I'm sorry. There is no way. That's just what you read in the paragraph above. Emailing anyone to ask for a specific version will just get the same answer, and will consume everyone's time. Please don't do it.
Which revision do I have?
There are three ways to tell which revision you have (and they should all match):
Look at the sticker
It's printed on the back of the Pluto SDR (on the sticker) the below in Rev B:
info.html page
In the file:///D:/info.html#version
page, it will tell you (assuming that your Pluto SDR drive is “D”):
Take it apart and look
The PCBs are slightly different (these pictures are the top sides).
If you look close, the revision of the PCB is etched in metal on the side (Zoomed in for clarity).
Revision C/D
Revision B
Although the below files indicates the Xilinx XC7Z010-1CLG225C
is used in the PlutoSDR, it is actually the Xilinx XC7Z010-1CLG225C4334
(a single core version before the 7007 was released). We keep using the “special” version. If you are starting a new design - use the XC7Z007S-1CLG225C
.
-
-
-
-
-
-
There are few pictures of rev B in the
Marketing section as well.
K
Why do a Rev C?
our “low-risk” OTG changes, caused problems, since we put the VBUS monitoring (R88) on the wrong side of the fuse, and the inclusion of the DC choke. While the DC choke reduces noise, and there is no DC difference between PGDN, and GND, on certain hosts, with certain operating systems, there can be a 250mV AC difference between PGND and GND. Since the analog comparators inside the Microchip USB3320 will be referenced to GND (quiet), it appears to toggle between host mode and device mode. A temp workaround was to change this resistor (R88) from the recommended
USB spec of 1k to 24.9k. R88 can be found on the back side, underneath the
USB connector.
We also had issue on
ESD testing, and will be adding an
ESD protection to the RF connector.
As a cost optimization (and feature enhancement), we may redo some of the power section (replacing the NCP339AFCT2G, ADM1177, with the
LTC4413) - this is still TBD based on lab work to be done. One of the usability issues - is that the 2 NCP339AFCT2G devices are designed to be break before make - which causes the power supply to reset if you plug the ADALM-PLUTO into a PC (which causes it to boot), and then eventually a power supply (which causes the supply to disappear for a small time, and then re-appear). We don't think this is a huge issue, but it would be enhance the usability. It would mean however, that we loose the ability to read
USB voltage/current (which we currently do in the
ADM1177.
Request to pin out the 2nd channel with pads/footprints.
Revision A
Why do a Rev B?
RF performance was bad. (EVM was poor, ~-32dBm; goal was -45dBm). This was due to the Rakon oscillator having no PPSR
1), and us powering the oscillator directly from a 1.8V digital rail (which was noisy). A LDO was
dead bugged onto rev A, and it fixed the performance problem. We tried a few L/C & ferrites, but it was not as good as the LDO, so we added an ultralow noise LDO, the
ADM7160ACPZN1.8 to the design.
RF performance was bad on certain PCs, even with with the added LDO (above). This was tracked down to to noise on the power supply. We added a power choke (DLW5BSM801TQ2L), and this went away, and we got much better results independent of platform.
Power supply noise was a little higher than we would have liked, and was effecting RF performance, so sync'ed the multiple switchers together to reduce input ripple. This also allowed us to reduce input capacitance on the entire unit.
were barely passing FCC, (due to noise @ 480MHz, which was also causing some RF issues at 480
MHz), so added DLW21HN900SQ2L (90Ω choke) on the
USB lines.
swapped QSPI flash and DDR3L devices, to something not on the obsolete list.
based on early end user feedback, added some test points to unused pins to make extending the device a little easier.
based on early end user feedback, added On-The-Go support for
USB. This was some minor power circuit, and monitoring VBUS, so was looked at as “low risk”
Before PlutoSDR
Like all things, PlutoSDR is a integration/copy/paste of previous known working platforms. There were a few different AD936x /Zynq platforms that were worked on that we borrowed things from:
-
FMCOMMS5 FMC Card, which is where we borrowed the (buggy) oscillator design, since the AD9363 can not be used with a crystal.
PicoZed SDR (which is were most of the Zynq and
USB comes from).