This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:tools:pluto:drivers:osx [07 Sep 2023 16:06] – [Mac OS X Drivers] Michael Hennerich | university:tools:pluto:drivers:osx [07 Sep 2023 16:17] (current) – [Ethernet] Remove HoRNDIS Michael Hennerich | ||
---|---|---|---|
Line 37: | Line 37: | ||
===== Ethernet ===== | ===== Ethernet ===== | ||
- | {{page>./ | + | <WRAP tip> |
+ | In order to use the ADALM-PLUTO (aka. PlutoSDR) or ADALM2000 (aka. M2k) with Mac OSX the ethernet compatibility mode must be set to **USB CDC-NCM**. | ||
- | Once the [[http:// | + | Please see instructions for [[:university: |
+ | </ | ||
- | <WRAP tip>You may need to reboot without the PlutoSDR plugged in, and then attach the PlutoSDR to get HoRNDIS to load properly< | + | {{page>./windows# |
- | {{: | + | You should see something like this when you goto -> System Preferences |
- | To check things out, it should look something like this in '' | + | {{:university: |
- | <WRAP box> | ||
- | < | ||
- | adi-mm: | ||
- | HoRNDIS: init: HoRNDIS tethering driver for Mac OS X, by Joshua Wise (rel8 final) | ||
- | HoRNDIS: probe: probe: came in with a score of 60000 | ||
- | HoRNDIS: message: unknown message type e000401f | ||
- | HoRNDIS: message: unknown message type e0000230 | ||
- | HoRNDIS: probe: probe: looks like we're good (2/2/255) | ||
- | USBMSC Identifier (non-unique): | ||
- | HoRNDIS: message: kIOMessageServiceIsAttemptingOpen | ||
- | HoRNDIS: openInterfaces: | ||
- | HoRNDIS: message: kIOMessageServiceIsAttemptingOpen | ||
- | HoRNDIS: rndisInit: their MTU 1486 | ||
- | HoRNDIS: setMaxTransferUnit: | ||
- | HoRNDIS: init: starting up with MTU 1486 | ||
- | en4: attached with 4 suspended link-layer multicast membership(s) | ||
- | HoRNDIS: message: kIOMessageServiceIsAttemptingOpen | ||
- | HoRNDIS: message: kIOMessageServiceIsRequestingClose | ||
- | HoRNDIS: message: kIOMessageServiceIsAttemptingOpen | ||
- | HoRNDIS: message: kIOMessageServiceIsRequestingClose | ||
- | en4: failed to restore 4 suspended link-layer multicast membership(s) (err=102) | ||
- | </ | ||
- | </ | ||
<WRAP box> | <WRAP box> |