This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:tools:pluto:devs:reboot [10 Jun 2019 06:46] – [Reboot to DFU-RAM] Robin Getz | university:tools:pluto:devs:reboot [17 Feb 2022 05:32] (current) – [Reboot to DFU-RAM] Robin Getz | ||
---|---|---|---|
Line 68: | Line 68: | ||
<WRAP top tip round box 100%>< | <WRAP top tip round box 100%>< | ||
- | Following commands can be used to boot a fresh build of the firmware image | + | Following commands can be used to boot a fresh build of the firmware image. To simply things, there is a script in [[github> |
< | < |