Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:tools:pluto:devs:reboot [10 Jun 2019 06:46]
Robin Getz [Reboot to DFU-RAM]
university:tools:pluto:devs:reboot [17 Feb 2022 05:32]
Robin Getz [Reboot to DFU-RAM]
Line 68: Line 68:
 <WRAP top tip round box 100%><​wrap info>​This specifies any shell prompt running on the development host</​wrap>​ <WRAP top tip round box 100%><​wrap info>​This specifies any shell prompt running on the development host</​wrap>​
  
-Following commands can be used to boot a fresh build of the firmware image+Following commands can be used to boot a fresh build of the firmware image. To simply things, there is a script in [[github>​plutosdr_scripts]] ''​pluto_ramboot''​ that can do all these steps in one command.
  
 <​xterm>​ <​xterm>​
university/tools/pluto/devs/reboot.txt · Last modified: 17 Feb 2022 05:32 by Robin Getz