This shows you the differences between two versions of the page.
— | university:tools:pluto:devs:port_forwarding [12 Oct 2019 00:52] (current) – created Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== Connecting your PlutoSDR to the Internet ====== | ||
+ | <WRAP important> | ||
+ | Do not do this, unless you have compiled custom firmware that does not use the default password. | ||
+ | </ | ||
+ | |||
+ | ====== Ports that are using on the PlutoSDR ====== | ||
+ | * 22 (ssh) | ||
+ | * 80 (http) | ||
+ | * 30431 (iiod) | ||
+ | |||
+ | ===== port forwarding ===== | ||
+ | |||
+ | You should not make port 30431 available on the internet, there is no security built into it, and anyone could change anything about your radio without you knowing about it. | ||
+ | |||
+ | If you need to run iio over the internet, set up a ssh tunnel, similar to this linux command: | ||
+ | < | ||
+ | rgetz@brain: | ||
+ | </ | ||
+ | |||
+ | This uses the following options: | ||
+ | ; **-n** : Redirects '' | ||
+ | ; **-N** : Do not execute a remote command. This is useful for just forwarding ports. | ||
+ | ; **-T** : Disable pseudo-terminal allocation. | ||
+ | ; **-L** : [bind_address: | ||
+ | |||
+ | This would allow anyone on your subnet to connect you your machine (use your IP) to connect to your PlutoSDR. |