Last revision Both sides next revision
university:tools:pluto:controlling_the_transceiver_and_transferring_data [28 Apr 2017 15:59]
Michael Hennerich [Controlling the transceiver]
university:tools:pluto:controlling_the_transceiver_and_transferring_data [28 Apr 2017 16:29]
Michael Hennerich [Controlling the transceiver]
Line 22: Line 22:
 It shows how to control the AD936x transceiver via a remote connection. It shows how to control the AD936x transceiver via a remote connection.
  
-  - Create IIO IP Network context. Instead of ip:​xxx.xxx.xxx.xxx it'll also accept usb:XX.XX.X+  - Create IIO IP Network context. Instead of ''​ip:​xxx.xxx.xxx.xxx'' ​it'll also accept ​''​usb:XX.XX.X''​
   - Get the AD936x PHY device structure   - Get the AD936x PHY device structure
-  - Find and write the TX LO frequency +  - Set the TX LO frequency ​(see [[resources:​tools-software:​linux-drivers:​iio-transceiver:​ad9361|AD9361 device driver documentation]]) ​ 
-  - Find and write RX baseband rate+  - Set RX baseband rate
    
 \\ \\
 <code c> <code c>
 +#include <​iio.h>​
 +
 int main (int argc, char **argv) int main (int argc, char **argv)
 { {
Line 46: Line 48:
  iio_device_find_channel(phy,​ "​voltage0",​ false),  iio_device_find_channel(phy,​ "​voltage0",​ false),
  "​sampling_frequency",​  "​sampling_frequency",​
- 50000000); /* RX baseband rate 50 MSPS */+ 5000000); /* RX baseband rate MSPS */
  
  receive(ctx);​  receive(ctx);​
Line 57: Line 59:
  
 ===== Receiving data ===== ===== Receiving data =====
 +
 +  - Get the RX capture device structure
 +  - Get the IQ input channels
 +  - Enable I and Q channel
 +  - Create the RX buffer
 +  - Fill the buffer ​
 +  - Process samples
 +
 +\\
  
 <code c> <code c>
university/tools/pluto/controlling_the_transceiver_and_transferring_data.txt · Last modified: 18 Dec 2020 17:55 by Rob Riggs