Wiki

The most recent version of this page is a draft.DiffThis version (12 Feb 2023 21:21) was approved by Robin Getz.The Previously approved version (11 Nov 2022 14:45) is available.Diff

This is an old revision of the document!


Building the Firmware Image

It is recommenced to use the pre-build images, which can be found at github.com/analogdevicesinc/plutosdr-fw/. These are build and tested by Analog Devices, and should work on your PlutoSDR without issues. If you want to change functionality, you will need to follow these instructions. To test your image, it is recommended to use the RAM Boot rather than writing to flash the first time. This keep the default firmware while you are testing your image, so if something goes wrong - its a quick power cycle to fix things.

Prerequisites

  1. Make sure to download, or upgrade your Sources
    • Make sure you have the recommended/required Vivado versions. It's likely listed in the archive section of the Xilinx web site. To check out what you need, look at the following tcl file (which was checked out in the sources link above).
      rgetz@brain:~/github/temp/plutosdr-fw$ grep -i REQUIRED_VIVADO_VERSION $(find ./ -name "adi*.tcl") | grep set
        set required_vivado_version "2021.1"
    • Depending on the version of Xilinx tools, you need to make sure that you have the 32-bit libraries (the Xilinx tools are distributed as 32-bit binaries).

This specifies any shell prompt running on your Linux development host

rgetz@brain:~/github/temp/plutosdr-fw$ find /opt/Xilinx/ -name vivado -executable -type f | xargs file | grep ELF
/opt/Xilinx/Vivado/2021.2/bin/unwrapped/lnx64.o/vivado: ELF 64-bit LSB executable, x86-64, version 1 (GNU/Linux), dynamically linked, interpreter /lib64/ld-linux-x86-64.so.2, for GNU/Linux 2.6.18, not stripped
If it reports as a 32-bit binary (which the above did not), and you are running on a 64-bit system, do:
michael@HAL9000:~/devel$ dpkg --add-architecture i386 
michael@HAL9000:~/devel$ apt-get update
michael@HAL9000:~/devel$ sudo apt-get install libc6:i386 libstdc++6:i386

There are a few other tools that are necessary in order to build your own Firmware Image.

This specifies any shell prompt running on your Linux development host

michael@HAL9000:~/devel$ sudo apt-get install git build-essential ccache device-tree-compiler dfu-util fakeroot help2man libncurses5-dev libssl1.0-dev mtools rsync u-boot-tools bc python cpio zip unzip file wget

Building

It is recommended that if you are building in a Virtual Machine (which is totally fine), the Base Memory be set to at least 4096 MBytes. The Xilinx Vivado tools require at least 1.6 Gig of memory when compile for the XC7Z010. It has been reported that 2048 Mbytes is not enough, and will cause the tools to hang.

Starting the build process is just a matter of typing make within the firmware repository. The Makefile requires a few environmental variables being set, and of course the ARM GCC toolchain in the PATH. Some paths maybe adjusted to match your Xilinx Vivado and Vitis install folders.

This specifies any shell prompt running on your Linux development host

michael@HAL9000:~/devel$ cd plutosdr-fw or m2k-fw
michael@HAL9000:~/devel/plutosdr-fw$ export CROSS_COMPILE=arm-linux-gnueabihf-
michael@HAL9000:~/devel/plutosdr-fw$ export PATH=$PATH:/opt/Xilinx/Vitis/2021.2/gnu/aarch32/lin/gcc-arm-linux-gnueabi/bin
michael@HAL9000:~/devel/plutosdr-fw$ export VIVADO_SETTINGS=/opt/Xilinx/Vivado/2021.2/settings64.sh
michael@HAL9000:~/devel/plutosdr-fw$ make

The initial build takes some time to complete, and also requires an INTERNET connection, since buildroot downloads the source packages from the WEB.

Depending on your distribution, you may need to force Vivado to use Gtk2. You can do that by adding:

This specifies any shell prompt running on your Linux development host

michael@HAL9000:~/devel/plutosdr-fw$ export SWT_GTK3=0

before you type make.

Build Artifacts

This specifies any shell prompt running on your Linux development host

      michael@HAL9000:~/devel/plutosdr-fw$ ls -AGhl build
      total 52M
      -rw-rw-r-- 1 michael   69 Apr 19 17:45 boot.bif
      -rw-rw-r-- 1 michael 446K Apr 19 17:45 boot.bin
      -rw-rw-r-- 1 michael 446K Apr 19 17:45 boot.dfu
      -rw-rw-r-- 1 michael 575K Apr 19 17:45 boot.frm
      -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.dfu
      -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.frm
      -rw-rw-r-- 1 michael   33 Apr 19 17:45 pluto.frm.md5
      -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.itb
      -rw-rw-r-- 1 michael  16M Apr 19 17:45 plutosdr-fw-v0.20.zip
      -rw-rw-r-- 1 michael 471K Apr 19 17:45 plutosdr-jtag-bootstrap-v0.20.zip
      -rw-r--r-- 1 michael 4,2M Apr 19 17:39 rootfs.cpio.gz
      drwxrwxr-x 6 michael 4,0K Apr 19 17:45 sdk
      -rw-rw-r-- 1 michael 940K Apr 19 17:45 system_top.bit
      -rw-rw-r-- 1 michael 362K Apr 19 17:45 system_top.hdf
      -rwxrwxr-x 1 michael 409K Apr 19 17:45 u-boot.elf
      -rw-rw---- 1 michael 128K Apr 19 17:45 uboot-env.bin
      -rw-rw---- 1 michael 129K Apr 19 17:45 uboot-env.dfu
      -rw-rw-r-- 1 michael 4,6K Apr 19 17:45 uboot-env.txt
      -rwxrwxr-x 1 michael 3,2M Apr 19 17:33 zImage
      -rw-rw-r-- 1 michael  16K Apr 19 17:39 zynq-pluto-sdr.dtb
      -rw-rw-r-- 1 michael  16K Apr 19 17:39 zynq-pluto-sdr-revb.dtb 

Testing on the target

There is a script in the plutosdr_scripts repo that will quickly download a build artifact (the pluto.dfu file) to an USB attached PlutoSDR. This will load the image into RAM, and not write to flash, enabling easy testing of images. However, since it is loading into RAM, it is not a persistent update over power cycles or further reboots.

This specifies any shell prompt running on your Linux development host

rgetz@brain:~/github/plutosdr-fw$ sudo ../plutosdr_scripts/pluto_ramboot
Found Pluto SDR at IP 192.168.3.1, running kernel:
	Linux pluto 5.4.0-00535-g9c04de11ae53 #1 SMP PREEMPT Fri Aug 20 13:01:03 CEST 2021 armv7l GNU/Linux
Found Pluto SDR in dfu mode and downloading ./build/pluto.dfu
successfully downloaded
Found new PlutoSDR at 192.168.3.1, running kernel:
	Linux pluto 5.4.0-00535-g9c04de11ae53 #1 SMP PREEMPT Tue Feb 15 16:17:50 EST 2022 armv7l GNU/Linux
rgetz@brain:~/github/plutosdr-fw$ 

Main targets

File Comment
pluto.frm Main PlutoSDR firmware file used with the USB Mass Storage Device
pluto.dfu Main PlutoSDR firmware file used in DFU mode
boot.frm First and Second Stage Bootloader (u-boot + fsbl + uEnv) used with the USB Mass Storage Device
boot.dfu First and Second Stage Bootloader (u-boot + fsbl) used in DFU mode
uboot-env.dfu u-boot default environment used in DFU mode
plutosdr-fw-vX.XX.zip ZIP archive containg all of the files above
plutosdr-jtag-bootstrap-vX.XX.zip ZIP archive containg u-boot and Vivao TCL used for JATG bootstrapping

Other intermediate targets

File Comment
boot.bif Boot Image Format file used to generate the Boot Image
boot.bin Final Boot Image
pluto.frm.md5 md5sum of the pluto.frm file
pluto.itb u-boot Flattened Image Tree
rootfs.cpio.gz The Root Filesystem archive
sdk Vivado/XSDK Build folder including the FSBL
system_top.bit FPGA Bitstream (from HDF)
system_top.hdf FPGA Hardware Description File exported by Vivado
u-boot.elf u-boot ELF Binary
uboot-env.bin u-boot default environment in binary format created form uboot-env.txt
uboot-env.txt u-boot default environment in human readable text format
zImage Compressed Linux Kernel Image
zynq-pluto-sdr.dtb Device Tree Blob for Rev.A
zynq-pluto-sdr-revb.dtb Device Tree Blob for Rev.B

How does it work

All these steps are automatically handled by make. They are just explained here, for those who are interested.

Build Linux kernel

Function File
PlutoSDR Linux Kernel Config zynq_pluto_defconfig
make -C linux ARCH=arm zynq_pluto_defconfig
make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zImage UIMAGE_LOADADDR=0x8000
cp linux/arch/arm/boot/zImage build/zImage

Making custom kernel changes

Normal users should not need to change their kernel, and this is only described for advanced users, or developers who periodically forget things

The command

make -C linux ARCH=arm zynq_pluto_defconfig

copies the file from arch/arm/configs/zynq_pluto_defconfig to .config and

make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zImage UIMAGE_LOADADDR=0x8000

builds it.

If you want to make a custom kernel, the easiest thing to do, is modify the .config with

make -C linux ARCH=arm zynq_pluto_defconfig
make -C linux ARCH=arm menuconfig

and then make changes, save them, and then create the defconfig.

make -C linux ARCH=arm savedefconfig

Check your changes against the default image

diff -u ./linux/arch/arm/configs/zynq_pluto_defconfig linux/defconfig | less

And if you are sure things are what you want, store them to the default file.

cp ./linux/defconfig ./linux/arch/arm/configs/zynq_pluto_defconfig

then this will work next time you type make to build the firmware image.

Build Devicetrees

Function File
PlutoSDR Rev.A Device Tree zynq-pluto-sdr.dts
PlutoSDR Rev.B Device Tree zynq-pluto-sdr-revb.dts
make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zynq-pluto-sdr.dtb
cp linux/arch/arm/boot/dts/zynq-pluto-sdr.dtb build/zynq-pluto-sdr.dtb

make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zynq-pluto-sdr-revb.dtb
cp linux/arch/arm/boot/dts/zynq-pluto-sdr-revb.dtb build/zynq-pluto-sdr-revb.dtb

Build Buildroot User Space

Function File
PlutoSDR Buildroot Config zynq_pluto_defconfig
make -C buildroot ARCH=arm zynq_pluto_defconfig
make -C buildroot TOOLCHAIN_EXTERNAL_INSTALL_DIR= ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- BUSYBOX_CONFIG_FILE=/home/michael/devel/pluto/plutosdr-fw/buildroot/board/pluto/busybox-1.25.0.config all
cp buildroot/output/images/rootfs.cpio.gz build/rootfs.cpio.gz

Configuring Buildroot

You need to copy over the correct file, to the .config, edit it (with menuconfig), and then save it to the right place so that the main build system will use the new file.

make -C buildroot ARCH=arm zynq_pluto_defconfig
make -C buildroot ARCH=arm menuconfig
make -C buildroot ARCH=arm savedefconfig
make

Build FPGA Hardware Description File

Function File
Pluto HDL Project Files
source /opt/Xilinx/Vivado/2021.2/settings64.sh
make -C hdl/projects/pluto
cp hdl/projects/pluto/pluto.sdk/system_top.hdf build/system_top.hdf

Build FPGA First Stage Bootloader (FSBL)

Function File
Create FSBL TCL script create_fsbl_project.tcl
source /opt/Xilinx/Vivado/2021.2/settings64.sh
xsdk -batch -source scripts/create_fsbl_project.tcl
cp build/sdk/hw_0/system_top.bit build/system_top.bit

Build multi component FIT image (Flattened Image Tree)

Function File
PlutoSDR Image Tree Source pluto.its
u-boot-xlnx/tools/mkimage -f scripts/pluto.its build/pluto.itb

Build Firmware DFU image

cp build/pluto.itb build/pluto.itb.tmp
dfu-suffix -a build/pluto.itb.tmp -v 0x0456 -p 0xb673
mv build/pluto.itb.tmp build/pluto.dfu

Build Firmware FRM image

md5sum build/pluto.itb | cut -d ' ' -f 1 > build/pluto.frm.md5
cat build/pluto.itb build/pluto.frm.md5 > build/pluto.frm

Build u-boot

Function File
PlutoSDR u-boot Config zynq_pluto_defconfig
PlutoSDR u-boot Device Tree zynq-pluto-sdr.dts
make -C u-boot-xlnx ARCH=arm zynq_pluto_defconfig
make -C u-boot-xlnx ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- UBOOTVERSION="PlutoSDR v0.20-PlutoSDR"
cp u-boot-xlnx/u-boot build/u-boot.elf

Build Zynq Boot Image

echo img:{[bootloader] build/sdk/fsbl/Release/fsbl.elf build/u-boot.elf } > build/boot.bif
source /opt/Xilinx/Vivado/2021.2/settings64.sh
bootgen -image build/boot.bif -w -o build/boot.bin

Build Boot DFU Image

cp build/boot.bin build/boot.bin.tmp
dfu-suffix -a build/boot.bin.tmp -v 0x0456 -p 0xb673
mv build/boot.bin.tmp build/boot.dfu

Build u-boot default environment Image

CROSS_COMPILE=arm-xilinx-linux-gnueabi- scripts/get_default_envs.sh > build/uboot-env.txt
u-boot-xlnx/tools/mkenvimage -s 0x20000 -o build/uboot-env.bin build/uboot-env.txt

Build u-boot default environment DFU Image

cp build/uboot-env.bin build/uboot-env.bin.tmp
dfu-suffix -a build/uboot-env.bin.tmp -v 0x0456 -p 0xb673
mv build/uboot-env.bin.tmp build/uboot-env.dfu

Build Boot FRM image

cat build/boot.bin build/uboot-env.bin scripts/target_mtd_info.key | tee build/boot.frm | md5sum | cut -d ' ' -f1 | tee -a build/boot.frm
/srv/wiki.analog.com/data/pages/university/tools/pluto/building_the_image.txt · Last modified: 15 Feb 2023 22:56 by Robin Getz