This is an old revision of the document!
The ADALM2000 (M2K) Active Learning Module is an affordable USB-powered data acquisition module that takes the capabilities of the ADALM1000 (M1K) Active Learning Module to the next level. With 12-bit ADCs(at 100MSPS) and DACs(at 150MSPS), the ADALM2000 with the Scopy software, brings the power of high performance lab equipment to the palm of your hand, enabling electrical engineering students and hobbyists to explore signals and systems into the tens of MHz without the cost and bulk associated with traditional lab gear. The ADALM2000, when coupled with Analog Devices' Scopy™ graphical application software running on a computer, provides the user with the following high performance instrumentation:
ADALM2000 is a portable lab. It's more than the combinations of a few parts, but to understand the capabilities of the unit, you must understand the fundamental operation of each part inside the unit. Depending on who you are, and what you want to do, you may have different needs, and different wants. It's expected that many people will stop when they solve their immediate problem and don't want to go any deeper into the stack. There are 3 main categories of users:
It's expected that most people will work their way down through each section, reading and skimming most of the content. The content is in a constant state of improvement, so if you do have a question, please ask at EngineerZone, or check the help and support page.
All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.
Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.