Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (31 Oct 2018 11:22) was approved by mhennerich.The Previously approved version (31 Oct 2018 10:45) is available.Diff

This is an old revision of the document!


ADALM2000 Overview

The ADALM2000 (M2K) Active Learning Module is an affordable USB-powered source-measurement unit that takes the capabilities of the ADALM1000 (M1K) Active Learning Module to the next level. With 12-bit ADCs and DACs running at 100 MSPS, the ADALM2000 brings the power of high performance lab equipment to the palm of your hand, enabling electrical engineering students and hobbyists to explore signals and systems into the tens of MHz without the cost and bulk associated with traditional lab gear. The ADALM2000, when coupled with Analog Devices' Scopy™ graphical application software running on a computer, provides the user with the following high performance instrumentation:

  • Two-channel oscilloscope with differential inputs
  • Two-channel arbitrary function generator
  • 16-channel digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)
  • 16-channel pattern generator (3.3V CMOS, 100MS/s)
  • 16-channel virtual digital I/O
  • Two input/output digital trigger signals for linking multiple instruments (3.3V CMOS)
  • Two-channel voltmeter (AC, DC, ±20V)
  • Network analyzer – Bode, Nyquist, Nichols transfer diagrams of a circuit. Range: 1Hz to 10MHz
  • Spectrum Analyzer – power spectrum and spectral measurements (noise floor, SFDR, SNR, THD, etc.)
  • Digital Bus Analyzers (SPI, I²C, UART, Parallel)
  • Two programmable power supplies (0…+5V , 0…-5V)

Introduction

ADALM2000 is a portable lab. It's more than the combinations of a few parts, but to understand the capabilities of the unit, you must understand the fundamental operation of each part inside the unit. Depending on who you are, and what you want to do, you may have different needs, and different wants. It's expected that many people will stop when they solve their immediate problem and don't want to go any deeper into the stack. There are 2 main categories of users:

    • ADALM2000 users normally interact with real world analog signals using Scopy or Alice
    • Everyone should read this section, as it describes the device, and describes how to get the drivers and host software installed properly.
    • normally write custom software or HDL (for the FPGA) that run directly on the ADALM2000 device. This may put the ADALM2000 in different modes, and support different external USB devices (including LAN (via USB), or WiFi (vs USB)), extending the capabilities of the device. This includes all the information to compile HDL projects, compile kernels, change to custom USB PID/VID and/or run custom user space applications.

It's expected that most people will work their way down through each section, reading and skimming most of the content. The content is in a constant state of improvement, so if you do have a question, please ask at EngineerZone, or check the help and support page.

All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.

Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.

university/tools/m2k.1540981364.txt.gz · Last modified: 31 Oct 2018 11:22 by mhennerich