Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
university:tools:m2k:tutorials:buildingaradiowithm2k [14 Jan 2020 07:22]
Pop Andreea Hardware setup-figures
university:tools:m2k:tutorials:buildingaradiowithm2k [25 Jan 2021 15:22] (current)
Adrian Suciu
Line 48: Line 48:
  
 =====Software===== =====Software=====
 +GNU Radio is a free and open-source software development toolkit that provides signal processing blocks to implement software radios. GNU Radio Companion (GRC) is a graphical tool for creating signal flow graphs and generating flow-graph source code.
 +GNU Radio can be extended with own functionality and blocks using OutOfTreeModules. gr-m2k is a module containing blocks for interfacing with ADALM2000.
 +
 +Creating a flowgraph in GRC, using GNU Radio 3.8, is an easy and fast solution. There are two possible approaches:
 +  * Creating a new out-of-tree module. Please check the available OutOfTreeModules [[https://​wiki.gnuradio.org/​index.php/​OutOfTreeModules#​Tools_and_resources_at_my_disposal|documentation]]
 +  * Integrating the ADF4350 block with gr-m2k
 +All steps for integrating ADF4350 with gr-m2k will be further explained.
 +
 +====  ADF4350 block ====
 +Controlling the radio implies controlling the output voltage frequency of ADF4350. A GRC block, integrated with M2k blocks, that controls the frequency can be created. no-OS provides a driver for ADF4350 that simplifies the work. This driver communicates using SPI. In the following steps we are going to create a GRC block for gr-m2k that uses libm2k communication segment integrated with no-OS drivers. ​
 +
 +  - Install libm2k. Instructions can be found [[/​university/​tools/​m2k/​libm2k/​libm2k|here]].
 +  - Compile the gr-m2k blocks for your PC. Check the steps [[/​university/​tools/​m2k/​libm2k/​gr-m2k|here]].
 +  - Download the ADF4350 driver from [[https://​github.com/​analogdevicesinc/​no-OS/​tree/​d00cc225a264d03807cafc4bf6a133af69affa36/​drivers/​frequency/​adf4350|no-OS page]].
 +
 +The steps to implement a GRC block:
 +  - Create the inclusion header
 +  - Create the implementation class
 +    - Add the driver
 +    - Implement the class
 +  - Create python bindings
 +  - Create the GRC component
 +
 +Project structure:
 +  * gr-m2k
 +    * grc
 +      * m2k_adf4350_sink.block.yml
 +    * include/m2k
 +      * adf4350_sink.h
 +    * lib
 +      * drivers
 +        * adf4350.h
 +        * adf4350.c
 +        * spi.h
 +      * adf4350_sink_impl.h
 +      * adf4350_sink_impl.cc
 +    * swig
 +      * m2k_swig.i
 +
 +
 +**Create the inclusion header**
 +
 +Create //​adf4350_sink.h//​ in gr-m2k/​include/​m2k.
 +
 +Add this file in the corresponding CMake file.
 +    install(FILES
 +    ...
 +    adf4350_sink.h
 +    DESTINATION ${GR_INCLUDE_DIR}/​m2k)
 +
 +In the make function add as parameters the URI and all attributes from the adf4350_init_param structure (23 attributes) found in the driver. This way they could be change from GRC without hard coding them.
 +
 +**Create the implementation class**
 +
 +In this part we are going to integrate libm2k with a no-OS driver. For more information please check this [[/​university/​tools/​m2k/​libm2k/​digital_communication#​libm2k_and_no-os_drivers|link]].
 +
 +Create //​adf4350_sink_impl.h//​ and //​adf4350_sink_impl.cc//​ in gr-m2k/lib.
 +Create a drives directory in gr-m2k/lib and add the ADF4350 driver. Add both source files in the corresponding CMake file.
 +    list(APPEND m2k_sources
 +    ...
 +    adf4350_sink_impl.cc
 +    drivers/​adf4350.c)
 +
 +Create a header called //spi.h// and include the SPI header of libm2k:
 +    //spi.h
 +    #include <​libm2k/​tools/​spi.hpp>​
 +
 +ADF4350 block will receive a message from a QT GUI block. The message contains the value of the frequency.
 +The adf4350_sink_impl class has to implement the class constructor and a method (//​write_attribute//​) that will receive the message and will communicate with the chip in order to set its output frequency.
 +
 +In the source file (//​adf4350_sink_impl.cc//​) include the SPI extra header of libm2k (//<​libm2k/​tools/​spi_extra.hpp>//​). In the constructor open the context and initialize m2k_spi_init structure :
 +    libm2k::​contexts::​M2k *context = analog_in_source_impl::​get_context(uri);​
 +    m2k_spi_init m2KSpiInit;
 +    m2KSpiInit.clock = 0;
 +    m2KSpiInit.mosi = 1;
 +    m2KSpiInit.miso = 7;
 +    m2KSpiInit.bit_numbering = MSB;
 +    m2KSpiInit.context = context;
 +
 +Initialize the adf4350 structure with the given parameters. The first parameter, spi_init_param,​ should contain these values:
 +    {
 +        1000000,
 +        2,
 +        SPI_MODE_0,
 +        (void*)&​m2KSpiInit
 +    }
 +
 +//​write_attribute//​ function is supposed to:
 +  * receive the message
 +  * convert it into a number
 +  * pass the value to the driver, in order to set the output frequency of ADF4350
 +
 +    pmt::pmt_t key;
 +    ​
 +    if (!is_pair(pdu)) {
 +        throw std::​runtime_error("​Message not a pair!\n"​);​
 +    }
 +    ​
 +    key = pmt::​car(pdu);​
 +    std::string skey = pmt::​symbol_to_string(key);​
 +    ​
 +    if (skey == "​frequency"​) {
 +        long long frequency;
 +        pmt::pmt_t freq = pmt::​cdr(pdu);​
 +        std::string sfreq = pmt::​symbol_to_string(freq);​
 +        frequency = std::​stoll(sfreq);​
 +        adf4350_out_altvoltage0_frequency(d_adf4350_device,​ frequency);
 +        std::cout << "​ADF4350:​ PLL 0 frequency = " << frequency << "​Hz."​ << std::endl;
 +    }
 +
 +**Create python bindings**
 +
 +In swig directory is a file called //​m2k_swig.i//​. Include the block'​s header in this file:
 +   %{
 +   ...
 +   #​include "​m2k/​adf4350_sink.h"​
 +   %}
 +   
 +   ...
 +   ​%include "​m2k/​adf4350_sink.h"​
 +   
 +   ...
 +   ​GR_SWIG_BLOCK_MAGIC2(m2k,​ adf4350_sink);​
 +
 +**Create the GRC component**
 +
 +GNU Radio 3.8 uses yml files for creating GRC blocks. Create a file //​m2k_adf4350_sink.block.yml//​ in the //grc// directory. This file will describe how the GRC block should look like.
 +Add all parameters using the following format:
 +    -   id: <key>
 +        label: <​name>​
 +        dtype: <​type>​
 +        default: <​value>​
 +        hide: part  # optional
 +
 +This block is a sink for messages, not streams. To specify this create the following tag:
 +    inputs:
 +      -   ​domain:​ message
 +          id: msg
 +          optional: false
 +
 +**Build the new created block**
 +    cd build
 +    cmake ..
 +    make
 +    sudo make install
 +    cd ../..
 +    sudo ldconfig
 +
 +The source code can be found on the gr-m2k [[https://​github.com/​analogdevicesinc/​gr-m2k|github page]]. In order to build it, make sure to enable digital option (cmake -DDIGITAL=ON ..).
 +
 +====  GNURadio-Companion Flowgraph ====
 +
 +{{:​university:​tools:​m2k:​tutorials:​m2k_fm.png|}}
 +
 +The file {{ :​university:​tools:​m2k:​tutorials:​m2k_fm.zip |}} contains the gnuradio flowgraph.
 +The gnuradio flowgraph acquires the data from the M2K and sets the ADF4350 PLL frequency. When changing the PLL frequency slider, the gnuradio ADF4350 block that we just written, encodes SPI messages to the PLL in order to change the frequency that is fed into the mixer. ​
 +The data acquired from the mixer is captured by the M2k using GNURadio. The flow then shifts the frequency by a smaller offset in the "​offset"​ slider. The offset slider allows fine tuning of the signal before it gets demodulated by the WBFM receiver block. Eventually the data is sent to an audio sink which plays back the radio in the speakers.
 +
 +This project was presented in GRCon 2019. Slides are available [[https://​www.gnuradio.org/​grcon/​grcon19/​presentations/​Building_a_radio_with_M2K_and_spare_parts/​|here]]
university/tools/m2k/tutorials/buildingaradiowithm2k.1578982941.txt.gz · Last modified: 14 Jan 2020 07:22 by Pop Andreea