This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
university:tools:m2k:scopy [31 Jul 2019 16:19] Guramulta Daniel Update installer links |
university:tools:m2k:scopy [08 Feb 2021 14:50] (current) Alexandra Trifan Update link to ADALM2000 for End users page |
||
---|---|---|---|
Line 2: | Line 2: | ||
===== About ===== | ===== About ===== | ||
- | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. | + | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. If you are interested in some [[./scopy/screen shots]] |
===== Download ===== | ===== Download ===== | ||
<WRAP round download> | <WRAP round download> | ||
Line 8: | Line 8: | ||
**Scopy for Windows ** | **Scopy for Windows ** | ||
* Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Installer for latest release (Windows 64/32-bit)]] | * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Installer for latest release (Windows 64/32-bit)]] | ||
- | * Download: [[https://tinyurl.com/yyfa4ytt| Installer for latest (nightly) build (Windows 64-bit)]] | ||
- | * Download: [[https://tinyurl.com/y3gj3547| Installer for latest (nightly) build (Windows 32-bit)]] | ||
**Scopy for Linux ** | **Scopy for Linux ** | ||
Line 16: | Line 14: | ||
**Scopy for OSX ** | **Scopy for OSX ** | ||
* Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| OSX installer]] | * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| OSX installer]] | ||
+ | |||
+ | **Scopy all platforms latest(nightly) builds ** | ||
+ | * Download: [[https://ci.appveyor.com/project/analogdevicesinc/scopy| Installer for latest (nightly) build]] | ||
+ | |||
</WRAP> | </WRAP> | ||
- | <WRAP round important>In order to have Scopy working with [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADALM2000.html|ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: | + | <WRAP round important>In order to have Scopy working with [[adi>ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: |
- | * [[university:tools:adalm2000:users|ADALM2000 for End Users]]. | + | * [[university:tools:m2k:users|ADALM2000 for End Users]]. |
</WRAP> | </WRAP> | ||
Line 26: | Line 28: | ||
=== Scopy for Windows === | === Scopy for Windows === | ||
Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | ||
+ | === Video === | ||
+ | {{youtube>894HkVXf7-U}} | ||
\\ | \\ | ||
=== Scopy for Linux === | === Scopy for Linux === | ||
- | Before downloading and extracting the scopy_v1.0-linux.zip archive, you need to setup Flatpak using [[https://flatpak.org/setup/ | this setup guide]] for your Linux distribution. | + | Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using [[https://flatpak.org/setup/ | this setup guide]] for your Linux distribution. |
For Ubuntu, you can use the following steps: | For Ubuntu, you can use the following steps: | ||
Line 42: | Line 45: | ||
<xterm> | <xterm> | ||
- | **flatpak install Scopy.flatpak** | + | **flatpak install scopy-v1.1.1-Linux-flatpak.flatpak** |
</xterm> | </xterm> | ||
+ | === Video === | ||
+ | {{youtube>9qgxmmTrcSE}} | ||
\\ | \\ | ||
=== Scopy for OSX === | === Scopy for OSX === | ||
Double click the downloaded .dmg to make its content available. "Scopy" will show up in the Finder sidebar and a window showing the content should open up. \\ | Double click the downloaded .dmg to make its content available. "Scopy" will show up in the Finder sidebar and a window showing the content should open up. \\ | ||
Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | ||
+ | |||
+ | === Video === | ||
+ | {{youtube>To0ACQ77tkg}} | ||
===== Launching ===== | ===== Launching ===== |