This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
university:tools:m2k:scopy [10 May 2018 13:57] Antoniu Miclaus edit |
university:tools:m2k:scopy [08 Feb 2021 14:50] (current) Alexandra Trifan Update link to ADALM2000 for End users page |
||
---|---|---|---|
Line 2: | Line 2: | ||
===== About ===== | ===== About ===== | ||
- | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. | + | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. If you are interested in some [[./scopy/screen shots]] |
===== Download ===== | ===== Download ===== | ||
<WRAP round download> | <WRAP round download> | ||
- | * **Scopy for Windows - Alpha Release** | + | |
- | * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Windows 32/64-bit installer]] | + | **Scopy for Windows ** |
- | * Download: [[https://ci.appveyor.com/api/projects/analogdevicesinc/scopy/artifacts/scopy-setup.exe?branch=master| Installer for latest (nightly) build (Windows 32/64-bit)]] | + | * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Installer for latest release (Windows 64/32-bit)]] |
+ | |||
+ | **Scopy for Linux ** | ||
+ | * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Scopy Flatpak installer]] | ||
+ | |||
+ | **Scopy for OSX ** | ||
+ | * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| OSX installer]] | ||
+ | |||
+ | **Scopy all platforms latest(nightly) builds ** | ||
+ | * Download: [[https://ci.appveyor.com/project/analogdevicesinc/scopy| Installer for latest (nightly) build]] | ||
</WRAP> | </WRAP> | ||
- | <WRAP round important>In order to have Scopy working with [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADALM2000.html|ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: | + | <WRAP round important>In order to have Scopy working with [[adi>ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: |
- | * [[university:tools:adalm2000:users|ADALM-2000 for End Users]]. | + | * [[university:tools:m2k:users|ADALM2000 for End Users]]. |
</WRAP> | </WRAP> | ||
===== Installation ===== | ===== Installation ===== | ||
+ | |||
+ | === Scopy for Windows === | ||
Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | ||
+ | === Video === | ||
+ | {{youtube>894HkVXf7-U}} | ||
+ | \\ | ||
+ | === Scopy for Linux === | ||
+ | Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using [[https://flatpak.org/setup/ | this setup guide]] for your Linux distribution. | ||
+ | |||
+ | For Ubuntu, you can use the following steps: | ||
+ | <xterm> | ||
+ | **sudo add-apt-repository ppa:alexlarsson/flatpak | ||
+ | sudo apt update | ||
+ | sudo apt install flatpak | ||
+ | flatpak remote-add --if-not-exists flathub https://flathub.org/repo/flathub.flatpakrepo** | ||
+ | </xterm> | ||
+ | |||
+ | After this, get the **Scopy.flatpak** file from the downloaded archive and run: | ||
+ | |||
+ | <xterm> | ||
+ | **flatpak install scopy-v1.1.1-Linux-flatpak.flatpak** | ||
+ | </xterm> | ||
+ | |||
+ | === Video === | ||
+ | {{youtube>9qgxmmTrcSE}} | ||
+ | \\ | ||
+ | === Scopy for OSX === | ||
+ | Double click the downloaded .dmg to make its content available. "Scopy" will show up in the Finder sidebar and a window showing the content should open up. \\ | ||
+ | Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | ||
+ | |||
+ | === Video === | ||
+ | {{youtube>To0ACQ77tkg}} | ||
+ | |||
===== Launching ===== | ===== Launching ===== | ||
- | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder (Scopy.exe).\\ | + | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder. \\ |
+ | |||
+ | On Linux, you can also run it using: | ||
+ | <xterm> | ||
+ | **flatpak run org.adi.Scopy** | ||
+ | </xterm> | ||
====== Using the Application ===== | ====== Using the Application ===== | ||
Line 71: | Line 118: | ||
Clicking the **Reset Scopy** button will reset the application to a default configuration. | Clicking the **Reset Scopy** button will reset the application to a default configuration. | ||
- | Checking the user notes preference will enable a tool where the user can add different pages with html formatted text | + | Checking the **user notes preference** will enable a tool where the user can add different pages with html formatted text |
<WRAP centeralign>{{:university:tools:m2k:notes1.png|}} | <WRAP centeralign>{{:university:tools:m2k:notes1.png|}} | ||
Line 77: | Line 124: | ||
\\ | \\ | ||
- | ===== Instruments ===== | + | ===== User Guides ===== |
Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, a list of instruments that are available for that device will be enabled. Each instrument can be opened from the left menu. | Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, a list of instruments that are available for that device will be enabled. Each instrument can be opened from the left menu. | ||
Line 84: | Line 131: | ||
The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | ||
- | <WRAP centeralign>{{:university:tools:m2k:scopy_instruments_menu.png| Scopy Home View}} | + | <WRAP centeralign>{{:university:tools:m2k:min_menu.png| Scopy Minimized Menu View}} |
</WRAP> | </WRAP> | ||
- | ==== Instruments User Guides ==== | + | === Detaching Instruments === |
+ | |||
+ | Scopy provides the detaching into multiple windows feature for each instrument available, providing a better view/manipulation. | ||
+ | |||
+ | There are 2 ways to do this: | ||
+ | - __Drag and Drop__ - select the desired instrument drag it outside Instrument Menu section and drop it inside the application window area. | ||
+ | |||
+ | <WRAP centeralign>{{:university:tools:m2k:scopy_drag_n_drop.gif| Scopy Drag and Drop}} | ||
+ | </WRAP> | ||
+ | |||
+ | - __Double Click__ - first make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it. | ||
+ | |||
+ | <WRAP centeralign>{{:university:tools:m2k:scopy_dc_detach.gif| Scopy Double Click Detach}} | ||
+ | </WRAP> | ||
+ | |||
+ | \\ | ||
+ | ==== Instruments Overview==== | ||
+ | |||
+ | <WRAP centeralign>{{:university:tools:m2k:scopy_instruments_menu.png| Scopy Home View}} | ||
+ | </WRAP> | ||
Complete user guides on how to use each Scopy instrument: | Complete user guides on how to use each Scopy instrument: | ||
Line 100: | Line 166: | ||
- [[university:tools:m2k:scopy:power-supply|Power Supply]] | - [[university:tools:m2k:scopy:power-supply|Power Supply]] | ||
+ | ==== Scripts ==== | ||
+ | |||
+ | User guide on how to use scripts with Scopy: | ||
+ | * [[university:tools:m2k:scopy:scripting-guide|Scopy - Scripting Guide]] | ||
\\ | \\ | ||
====== Building ====== | ====== Building ====== | ||
Line 106: | Line 176: | ||
- [[university:tools:m2k:scopy:build-windows|Windows]] | - [[university:tools:m2k:scopy:build-windows|Windows]] | ||
- [[university:tools:m2k:scopy:build-linux|Linux]] | - [[university:tools:m2k:scopy:build-linux|Linux]] | ||
+ | - [[university:tools:m2k:scopy:build-osx|OSX]] | ||