This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy [04 May 2018 11:48] – Antoniu Miclaus | university:tools:m2k:scopy [10 May 2018 13:57] – edit Antoniu Miclaus | ||
---|---|---|---|
Line 9: | Line 9: | ||
* Download: [[https:// | * Download: [[https:// | ||
</ | </ | ||
+ | |||
<WRAP round important> | <WRAP round important> | ||
* [[university: | * [[university: | ||
Line 22: | Line 23: | ||
===== Home ===== | ===== Home ===== | ||
- | The Home view is divided into three sections: | + | The Home view is divided into four sections: |
- | * **Devices**: | + | * **Devices(1)**: List of devices (USB or remote) that Scopy can connect to. USB devices are detected automatically at startup. The __Add__ button can be used to add remote devices to the list. |
- | * **Instruments Menu**: List with instruments provided by the application. | + | * **Instruments Menu(2)**: List with instruments provided by the application. |
- | * **Information Window**: | + | * **Information Window(3)**: Section containing the welcome, add device |
+ | * **General Settings Menu(4)**: Save and load session and the preferences menu. | ||
- | {{ : | + | <WRAP centeralign> |
+ | </ | ||
- | \\ | ||
==== Connecting to a USB device ==== | ==== Connecting to a USB device ==== | ||
- | If a compatible USB device is available it will be displayed | + | If a compatible USB device is available it will be displayed |
- | To connect to that device click on the device and then click the **Connect** button. If the connection was established, | + | |
- | {{ : | + | To connect to that device click on the device and then click the **Connect** button in the **Information Window**. |
- | \\ | + | If the connection was established, |
- | ==== Connecting to a remote | + | |
- | To connect to a remote device click on the **Plus** icon. Enter the IP of the remote device into the **Hostname** field and click the **Connect** button. If a device can be detected at the IP you provided, the **Connect** button will change to an **Add** button and you can click on it to add the remote device to the list of detected devices. | + | <WRAP centeralign> |
- | The last step is to click on the icon of the remote device and click on the **Connect** button. | + | </ |
- | {{ : | + | ==== Connecting to a remote device ==== |
+ | To connect to a remote device click on the **Plus** icon. Enter the IP of the remote device into the **Hostname** field and click the **Connect** button. If a device can be detected at the IP you provided, the **Connect** button will change to an **Add** button and you can click on it to add the remote device to the list of detected devices. | ||
\\ | \\ | ||
- | ===== Instruments Menu ===== | + | <WRAP centeralign> |
+ | </ | ||
- | Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, | + | <WRAP centeralign> |
- | The icon on the right of the instrument name specifies that the instrument is enabled and provides a shortcut that allows an instrument to be turned on or off. | + | </ |
- | The instruments menu can be minimized by clicking on the **Scopy** button | + | Clicking |
- | {{ : | + | Clicking the **Identify** button will make the device blink. |
\\ | \\ | ||
- | ===== Digital IO ===== | ||
- | Digital IO details are available [[university: | + | ===== General Settings Menu ===== |
- | \\ | + | <WRAP centeralign> |
+ | </ | ||
- | ===== Voltmeter ===== | + | The save/load buttons can be used to save the current session or load another session. |
+ | The preferences button will open the preferences for Scopy where different options for different tools can be modified. | ||
- | Voltmeter details are available [[university: | + | <WRAP centeralign> |
+ | </ | ||
- | \\ | + | Clicking the **Reset Scopy** button will reset the application to a default configuration. |
- | ===== Oscilloscope ===== | + | |
- | Oscilloscope details are available [[university: | + | |
- | \\ | + | Checking the user notes preference will enable a tool where the user can add different pages with html formatted text |
- | ===== Signal Generator ===== | + | |
- | Signal Generator details are available [[university: | + | |
- | \\ | + | <WRAP centeralign> |
- | ===== Power Supply ===== | + | </ |
- | Power Supply details are available [[university: | + | |
\\ | \\ | ||
- | ===== Pattern Generator | + | ===== Instruments |
- | Pattern Generator details are available [[university: | + | |
- | \\ | + | Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, |
+ | The icon on the right of the instrument name specifies that the instrument is enabled and provides a shortcut that allows an instrument to be turned on or off. | ||
- | ===== Logic Analyzer ===== | + | The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. |
- | Logic Analyzer details are available [[university: | + | |
- | \\ | + | <WRAP centeralign> |
+ | </ | ||
- | ===== Network Analyzer | + | ==== Instruments User Guides |
- | Network Analyzer details are available [[university: | + | |
- | \\ | + | Complete user guides on how to use each Scopy instrument: |
- | ===== Spectrum Analyzer | + | - [[university: |
- | Spectrum | + | - [[university: |
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
\\ | \\ | ||
====== Building ====== | ====== Building ====== | ||
- | ===== Linux ===== | + | |
- | For building | + | Complete |
- | \\ | + | - [[university: |
- | ===== Windows ===== | + | |
- | For building Scopy on Windows, use the steps defined | + | |
Line 107: | Line 111: | ||
====== Source code ====== | ====== Source code ====== | ||
- | The source code for the entire application | + | The source code for the entire application |