university:tools:m2k:scopy [31 Jul 2019 16:19]
Guramulta Daniel Update installer links
university:tools:m2k:scopy [08 Feb 2021 14:50]
Alexandra Trifan Update link to ADALM2000 for End users page
Line 2: Line 2:
  
 ===== About ===== ===== About =====
-Scopy is a multi-functional software toolset with strong capabilities for signal analysis.+Scopy is a multi-functional software toolset with strong capabilities for signal analysis. ​If you are interested in some [[./​scopy/​screen shots]]
 ===== Download ===== ===== Download =====
 <WRAP round download>​ <WRAP round download>​
Line 8: Line 8:
 **Scopy for Windows ** **Scopy for Windows **
   * Download: [[https://​github.com/​analogdevicesinc/​scopy/​releases/​latest| Installer for latest release (Windows 64/​32-bit)]]   * Download: [[https://​github.com/​analogdevicesinc/​scopy/​releases/​latest| Installer for latest release (Windows 64/​32-bit)]]
-  * Download: [[https://​tinyurl.com/​yyfa4ytt| Installer for latest (nightly) build (Windows 64-bit)]] 
-  * Download: [[https://​tinyurl.com/​y3gj3547| Installer for latest (nightly) build (Windows 32-bit)]] 
  
 **Scopy for Linux ** **Scopy for Linux **
Line 16: Line 14:
 **Scopy for OSX ** **Scopy for OSX **
   * Download: [[https://​github.com/​analogdevicesinc/​scopy/​releases/​latest| OSX installer]]   * Download: [[https://​github.com/​analogdevicesinc/​scopy/​releases/​latest| OSX installer]]
 +
 +**Scopy all platforms latest(nightly) builds **
 +  * Download: [[https://​ci.appveyor.com/​project/​analogdevicesinc/​scopy| Installer for latest (nightly) build]]
 +
 </​WRAP>​ </​WRAP>​
  
-<WRAP round important>​In order to have Scopy working with [[http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​ADALM2000.html|ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: +<WRAP round important>​In order to have Scopy working with [[adi>ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: 
-  * [[university:​tools:​adalm2000:​users|ADALM2000 for End Users]].+  * [[university:​tools:​m2k:​users|ADALM2000 for End Users]].
 </​WRAP>​ </​WRAP>​
  
Line 26: Line 28:
 === Scopy for Windows === === Scopy for Windows ===
 Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required.
 +=== Video ===  
 +{{youtube>​894HkVXf7-U}}
 \\ \\
 === Scopy for Linux === === Scopy for Linux ===
-Before downloading and extracting the scopy_v1.0-linux.zip archive, you need to setup Flatpak using [[https://​flatpak.org/​setup/​ | this setup guide]] for your Linux distribution.+Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using [[https://​flatpak.org/​setup/​ | this setup guide]] for your Linux distribution.
  
 For Ubuntu, you can use the following steps: For Ubuntu, you can use the following steps:
Line 42: Line 45:
  
 <​xterm>​ <​xterm>​
-    **flatpak install ​Scopy.flatpak**+    **flatpak install ​scopy-v1.1.1-Linux-flatpak.flatpak**
 </​xterm>​ </​xterm>​
  
 +=== Video === 
 +{{youtube>​9qgxmmTrcSE}}
 \\ \\
 === Scopy for OSX === === Scopy for OSX ===
 Double click the downloaded .dmg to make its content available. "​Scopy"​ will show up in the Finder sidebar and a window showing the content should open up. \\ Double click the downloaded .dmg to make its content available. "​Scopy"​ will show up in the Finder sidebar and a window showing the content should open up. \\
 Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\
 +
 +=== Video === 
 +{{youtube>​To0ACQ77tkg}}
  
 ===== Launching ===== ===== Launching =====
university/tools/m2k/scopy.txt · Last modified: 08 Feb 2021 14:50 by Alexandra Trifan