Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
university:tools:m2k:scopy [30 May 2018 15:47] – Remove references to alpha version Adrian Suciuuniversity:tools:m2k:scopy [04 Feb 2021 11:14] – [Download] Adrian Suciu
Line 2: Line 2:
  
 ===== About ===== ===== About =====
-Scopy is a multi-functional software toolset with strong capabilities for signal analysis.+Scopy is a multi-functional software toolset with strong capabilities for signal analysis. If you are interested in some [[./scopy/screen shots]]
 ===== Download ===== ===== Download =====
 <WRAP round download> <WRAP round download>
-  * **Scopy for Windows ** 
-  * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Windows 32/64-bit installer]] 
-  * Download: [[https://ci.appveyor.com/api/projects/analogdevicesinc/scopy/artifacts/scopy-setup.exe?branch=master| Installer for latest (nightly) build (Windows 32/64-bit)]] 
  
-  * **Scopy for Linux **+**Scopy for Windows ** 
 +  * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Installer for latest release (Windows 64/32-bit)]] 
 + 
 +**Scopy for Linux **
   * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Scopy Flatpak installer]]   * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Scopy Flatpak installer]]
  
-  * **Scopy for OSX **+**Scopy for OSX **
   * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| OSX installer]]   * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| OSX installer]]
 +
 +**Scopy all platforms latest(nightly) builds **
 +  * Download: [[https://ci.appveyor.com/project/analogdevicesinc/scopy| Installer for latest (nightly) build]]
 +
 </WRAP> </WRAP>
  
-<WRAP round important>In order to have Scopy working with [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADALM2000.html|ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: +<WRAP round important>In order to have Scopy working with [[adi>ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: 
-  * [[university:tools:adalm2000:users|ADALM-2000 for End Users]].+  * [[university:tools:adalm2000:users|ADALM2000 for End Users]].
 </WRAP> </WRAP>
  
Line 24: Line 28:
 === Scopy for Windows === === Scopy for Windows ===
 Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required.
 +=== Video ===  
 +{{youtube>894HkVXf7-U}}
 \\ \\
 === Scopy for Linux === === Scopy for Linux ===
-Before downloading and extracting the scopy_v1.0-linux.zip archive, you need to setup Flatpak using [[https://flatpak.org/setup/ | this setup guide]] for your Linux distribution.+Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using [[https://flatpak.org/setup/ | this setup guide]] for your Linux distribution.
  
 For Ubuntu, you can use the following steps: For Ubuntu, you can use the following steps:
Line 40: Line 45:
  
 <xterm> <xterm>
-    **flatpak install Scopy.flatpak**+    **flatpak install scopy-v1.1.1-Linux-flatpak.flatpak**
 </xterm> </xterm>
  
 +=== Video === 
 +{{youtube>9qgxmmTrcSE}}
 \\ \\
 === Scopy for OSX === === Scopy for OSX ===
 Double click the downloaded .dmg to make its content available. "Scopy" will show up in the Finder sidebar and a window showing the content should open up. \\ Double click the downloaded .dmg to make its content available. "Scopy" will show up in the Finder sidebar and a window showing the content should open up. \\
 Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\
 +
 +=== Video === 
 +{{youtube>To0ACQ77tkg}}
  
 ===== Launching ===== ===== Launching =====
Line 114: Line 124:
  
 \\ \\
-===== Instruments =====+===== User Guides =====
  
 Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, a list of instruments that are available for that device will be enabled. Each instrument can be opened from the left menu. Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, a list of instruments that are available for that device will be enabled. Each instrument can be opened from the left menu.
Line 121: Line 131:
 The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window.
  
-<WRAP centeralign>{{:university:tools:m2k:scopy_instruments_menu.png| Scopy Home View}}+<WRAP centeralign>{{:university:tools:m2k:min_menu.png| Scopy Minimized Menu View}}
 </WRAP> </WRAP>
  
-==== Instruments User Guides ====+=== Detaching Instruments === 
 + 
 +Scopy provides the detaching into multiple windows feature for each instrument available, providing a better view/manipulation. 
 + 
 +There are 2 ways to do this: 
 +  - __Drag and Drop__ - select the desired instrument drag it outside Instrument Menu section and drop it inside the application window area. 
 + 
 +<WRAP centeralign>{{:university:tools:m2k:scopy_drag_n_drop.gif| Scopy Drag and Drop}} 
 +</WRAP> 
 + 
 +  - __Double Click__ - first make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it.  
 + 
 +<WRAP centeralign>{{:university:tools:m2k:scopy_dc_detach.gif| Scopy Double Click Detach}} 
 +</WRAP> 
 + 
 +\\ 
 +==== Instruments Overview==== 
 + 
 +<WRAP centeralign>{{:university:tools:m2k:scopy_instruments_menu.png| Scopy Home View}} 
 +</WRAP>
  
 Complete user guides on how to use each Scopy instrument: Complete user guides on how to use each Scopy instrument:
Line 137: Line 166:
   - [[university:tools:m2k:scopy:power-supply|Power Supply]]   - [[university:tools:m2k:scopy:power-supply|Power Supply]]
  
 +==== Scripts ====
 +
 +User guide on how to use scripts with Scopy:
 +  * [[university:tools:m2k:scopy:scripting-guide|Scopy - Scripting Guide]]
 \\ \\
 ====== Building ====== ====== Building ======
university/tools/m2k/scopy.txt · Last modified: 28 Sep 2022 22:11 by Adrian Suciu