Description | Test Steps | Steps Resources | Expected Results |
Checking individual digital pin state | 1. Set DIO 0-7 and DIO 8-15 as individual pins | | The interface should look like in the “Step Resources” picture (left side). |
2. Set channel 0 as output | | The interface should look like in the “Step Resources” picture (left side). |
3. Set channel 7 as input | | The interface should look like in the “Step Resources” picture (left side). |
4. Connect digital channel 0 to channel 7 via wires. | | |
5. Change the logic state of channel 0 (0/1) multiple times and monitor channel 7 state. | | When channel 0 is set to logic one, channel 7 will be automatically set to logic 1. When channel 0 is set to logic one, channel 7 will be automatically set to logic 1. |
6. Connect the channel 0 to voltmeter and channel 7 to the positive power supply. | | |
7. Set channel 0 to logic state 0. | | The interface should look like in the “Step Resources” picture (left side). |
8. Monitor the voltage value via voltmeter. | | On the voltmeter the voltage displayed is be between -0.050V and 0.4V. |
9. Set channel 0 to logic state 1. | | The interface should look like in the “Step Resources” picture (left side). |
10. Monitor the voltage value via voltmeter. | | On the voltmeter the voltage displayed should be between 2.9V and 3.4V. |
11. Set positive power supply to voltage level between 0V and 0.8V. | | The interface should look like in the “Step Resources” picture (left side). |
12. Monitor the channel 7 logic state. | | Channel 7 indicates logic 0 level. |
13. Set positive power supply to voltage level between 2V and 3.3V | | The interface should look like in the “Step Resources” picture (left side). |
14. Monitor the channel 7 logic state. | | Channel 7 indicates logic 1 level. |
15. In step 2 replace by turn channel 0 with channels from 1 to 6 and from 8 to 15. Then, for each replacement repeat steps from 3 to 13. | | |
16. In step 2 replace with channel 7 and in step 3 by turn channels from 0 to 6 and from 8 to 15. Then, for each replacement repeat steps from 4 to 13. | | |