Wiki

This version (06 Dec 2018 15:30) was approved by Antoniu Miclaus.The Previously approved version (03 Jul 2018 13:54) is available.Diff

This is an old revision of the document!


Scopy - Scripting Guide

Important! The following guide in experimental phase, therefore no guarantee is offered regarding its functionality.

How to Use

Scopy tool supports scripting via javascript files, offering the possibility of automating instrument tasks for different types of applications (i.e control loops).

The scripts can be run in two different ways:

Via command line:

         scopy --script my_script.js

Via Debugger Instrument

To open the Debugger in Scopy tool, its visibility must be enbled in the Instrument Menu. To do this, open the Scopy.ini file under the following path: “C:\Users\<your_username>\AppData\Roaming\ADI”. Change the “debugger” property from the “launcher” group from 'false' to 'true. Make sure that Scopy app is closed when doing the file modifications.

Now open Scopy:


Connect to ADALM2000 device and open the Debugger Instrument.

To load a script press “Load Script” button and select the folder path of the file.


After the location is set, to run the script press the “Run” button placed on the left side of the “Load Script” button.

Available Commands

A list of supported commands by the Scopy tool.

General

Command Permission Description
exit() Write Exit Scopy application.
msleep(ms) Write Delay for a specific amount of time (specified in milliseconds).
printToConsole(value) Write Print value to the console.
fileIO.writeToFile(value,path) Write Write value in a file at specified path.
fileIO.appendToFile(value,path) Write Append value in a file at specified path.
fileIO.readAll(path) Read Read content from a file at specified path.
fileIO.readLine(path,lineNr) Read Read entire line form a file at specified path.

DigitalIO

Command Permission Values Description
dio.dir[idx] Read/Write true(out);false(in) Set channel direction (idx=0-15)
dio.out[idx] Read/Write true(high);false(low) Set channel output (idx=0-15)
dio.gpi[idx] Read true(high);false(low) Check pin value (high/low)
dio.running Read/Write true(on);false(off) Run DigitalIO instrument

Power Supply

Command Permission Values Description
power.sync Read/Write true(track);false(independent) Set Power Supplies as Independent or Tracking control.
power.tracking_percent Read/Write 0 - 100 (%) Set Power Supplies Tracking ratio.
power.dac1_enabled Read/Write true(on);false(off) Enable/Disable Positive Power Supply.
power.dac2_enabled Read/Write true(on);false(off) Enable/Disable Negative Power Supply.
power.dac1_value Read/Write 0 - 5 (V) Set Positive Power Supply output value.
power.dac2_value Read/Write (-5) - 0(V) Set Negative Power Supply output value.

Voltmeter

Command Permission Values Description
dmm.mode_ac_low_ch1 Read/Write true(on);false(off) Set Channel 1 to AC mode (20Hz-800Hz)
dmm.mode_ac_low_ch2 Read/Write true(on);false(off) Set Channel 2 to AC mode (20Hz-800Hz)
dmm.mode_ac_high_ch1 Read/Write true(on);false(off) Set Channel 1 to AC mode (800Hz-40kHz)
dmm.mode_ac_high_ch2 Read/Write true(on);false(off) Set Channel 2 to AC mode (800Hz-40kHz)
dmm.histogram_ch1 Read/Write true(on);false(off) Enable/Disable Channel 1 History plot.
dmm.histogram_ch2 Read/Write true(on);false(off) Enable/Disable Channel 2 History plot.
dmm.history_ch1_size_idx Read/Write 0 - 2 Channel 1 History plot size(1s,10s,60s).
dmm.history_ch2_size_idx Read/Write 0 - 2 Channel 2 History plot size(1s,10s,60s).
dmm.value_ch1 Read Volts Read Channel 1 value.
dmm.value_ch2 Read Volts Read Channel 2 value.
dmm.peak_hold_en Read/Write true(on);false(off) Enable/Disable Peak Hold.
dmm.data_logging_en Read/Write true(on);false(off) Enable/Disable Data Logging.
dmm.data_logging_timer Read/Write 0 - 3600(s) Set Data Logging Time.
dmm.data_logging_append Read/Write true(append);false(overwrite) Overwrite/Append data logging to file
dmm.running Read/Write true(on);false(off) Run Voltmeter instrument

Signal Generator

Command Permission Values Description
siggen.mode[idx] Read/Write 0 - 3 Set Channel 1/2 (idx=0/1) Operation mode (Constant, Waveform, Buffer, Math).
siggen.constant_volts[idx] Read/Write (-5) - 5 (V) Set Channel 1/2 (idx=0/1) voltage in Constant Mode.
siggen.waveform_type[idx] Read/Write 0 - 5 Set Channel 1/2 (idx=0/1) waveform type in Waveform Mode (Sine, Square, Triangle, Trapezoidal, Rising Ramp Sawtooth, Falling Ramp Sawtooth).
siggen.waveform_amplitude[idx] Read/Write 0.000001 - 5 (V) Set Channel 1/2 (idx=0/1) waveform amplitude in Waveform Mode.
siggen.waveform_frequency[idx] Read/Write 0.001 - 37500000 (Hz) Set Channel 1/2 (idx=0/1) waveform frequency in Waveform Mode.
siggen.waveform_offset[idx] Read/Write (-5) - 5 (V) Set Channel 1/2 (idx=0/1) waveform offset in Waveform Mode.
siggen.waveform_phase[idx] Read/Write 0 - 359 (deg) Set Channel 1/2 (idx=0/1) waveform phase in Waveform Mode.
siggen.waveform_duty[idx] Read/Write 0 - 100 (%) Set Channel 1/2 (idx=0/1) waveform duty in Waveform Mode (Square).
siggen.waveform_rise[idx] Read/Write 0.00000001 - 10 (s) Set Channel 1/2 (idx=0/1) waveform rise time in Waveform Mode (Trapezoidal).
siggen.waveform_fall[idx] Read/Write 0.00000001 - 10 (s) Set Channel 1/2 (idx=0/1) waveform fall time in Waveform Mode (Trapezoidal).
siggen.waveform_holdhigh[idx] Read/Write 0.00000001 - 10 (s) Set Channel 1/2 (idx=0/1) waveform high time in Waveform Mode (Trapezoidal).
siggen.waveform_holdlow[idx] Read/Write 0.00000001 - 10 (s) Set Channel 1/2 (idx=0/1) waveform low time in Waveform Mode (Trapezoidal).
siggen.noise_type[idx] Read/Write 0(None); 200 - 203 Set Channel 1/2 (idx=0/1) Noise Type (None, Uniform, Gaussian, Laplacian, Impulse).
siggen.noise_amplitude[idx] Read/Write 0.000001 - 10 (V) Set Channel 1/2 (idx=0/1) Noise Amplitude.
siggen.math_function[idx] Read/Write String Set Channel 1/2 (idx=0/1) Math function.
siggen.math_frequency[idx] Read/Write 0.001 - 37500000 (Hz) Set Channel 1/2 (idx=0/1) Math frequency.
siggen.buffer_file_path[idx] Read/Write String Set Channel 1/2 (idx=0/1) Buffer file Path.
siggen.buffer_amplitude[idx] Read/Write 0.000000001 - 10 (V) Set Channel 1/2 (idx=0/1) Buffer amplitude.
siggen.buffer_offset[idx] Read/Write (-5) - 5 (V) Set Channel 1/2 (idx=0/1) Buffer offset.
siggen.buffer_sample_rate[idx] Read/Write 0.1 - 37500000 (V) Set Channel 1/2 (idx=0/1) Buffer sample rate.
siggen.buffer_phase[idx] Read/Write 0 - 359 (deg) Set Channel 1/2 (idx=0/1) Buffer phase.
siggen.enabled[idx] Read/Write true(on);false(off) Enabled/Disable Channel 1/2 (idx=0/1)
siggen.running Read/Write true(on);false(off) Run Signal Generator instrument.

Network Analyzer

Command Permission Values Description
network.min_freq Read/Write 1 - 30000000 (Hz) Set Sweep Minimum Frequency.
network.max_freq Read/Write 1 - 30000000 (Hz) Set Sweep Maximum Frequency.
network.samples_count Read/Write 10 - 1000 (samples) Set Sweep Samples Count.
network.amplitude Read/Write 0.000001 - 10 (V) Set Waveform Amplitude.
network.offset Read/Write (-5) - 5 (V) Set Waveform Offset.
network.min_mag Read/Write (-120) - 120 (dB) Set Minimum Magnitude displayed.
network.max_mag Read/Write (-120) - 120 (dB) Set Maximum Magnitude displayed.
network.min_phase Read/Write (-180) - 180 (deg) Set Minimum Phase displayed.
network.max_phase Read/Write (-180) - 180 (deg) Set Maximum Phase displayed.
network.log_freq Read/Write true(log)/false(lin) Set Logarithmic/Linear plot scale display.
network.ref_channel Read/Write 1;2 Set Channel 1/2 as reference channel.
network.line_thickness Read/Write 0-9 Set plot line thickness (0.5, 1, 1.5, 2, 2.5, 3, 3.5, 4, 4.5, 5)
network.cursors Read/Write true(on);false(off) Enable/Disable Plot Cursors.
network.cursors_position Read/Write 0 - 3 Change Cursors Table position on plot.
network.cursors_transparency Read/Write 0 - 100 (%) Change Cursors Table transparency on plot.
network.running Read/Write true(on);false(off) Run Network Analyzer instrument.

Oscilloscope

Command Permission Values Description
osc.channels[idx].enabled Read/Write true(on);false(off) Enable/Disable Channel 1/2 (idx=0/1)
osc.channels[idx].volts_per_div Read/Write 0.001 - 10 (V) Set Channel 1/2 (idx=0/1) Volts/Div value for the plot.
osc.channels[idx].ac_coupling Read/Write true(on); false(off) Enable/Disable Channel 1/2 (idx=0/1) AC Coupling.
osc.channels[idx].period Read (s) Read Channel 1/2 (idx=0/1) signal's period.
osc.channels[idx].mean Read (V) Read Channel 1/2 (idx=0/1) signal's mean value.
osc.channels[idx].cycle_mean Read (V) Read Channel 1/2 (idx=0/1) signal's cycle mean value.
osc.channels[idx].rms Read (V) Read Channel 1/2 (idx=0/1) signal's RMS value.
osc.channels[idx].cycle_rms Read (V) Read Channel 1/2 (idx=0/1) signal's Cycle RMS value.
osc.channels[idx].ac_rms Read (V) Read Channel 1/2 (idx=0/1) signal's AC RMS value.
osc.channels[idx].area Read (V) Read Channel 1/2 (idx=0/1) signal's Area value.
osc.channels[idx].cycle_area Read (V) Read Channel 1/2 (idx=0/1) signal's Cycle Area value.
osc.channels[idx].min Read (V) Read Channel 1/2 (idx=0/1) signal's min value.
osc.channels[idx].max Read (V) Read Channel 1/2 (idx=0/1) signal's max value.
osc.channels[idx].amplitude Read (V) Read Channel 1/2 (idx=0/1) signal's amplitude value.
osc.channels[idx].peak_to_peak Read (V) Read Channel 1/2 (idx=0/1) signal's peak-to-peak value.
osc.channels[idx].low Read (V) Read Channel 1/2 (idx=0/1) signal's low value.
osc.channels[idx].high Read (V) Read Channel 1/2 (idx=0/1) signal's high value.
osc.channels[idx].middle Read (V) Read Channel 1/2 (idx=0/1) signal's middle value.
osc.channels[idx].pos_overshoot Read (%) Read Channel 1/2 (idx=0/1) signal's positive overshoot value.
osc.channels[idx].neg_overshoot Read (%) Read Channel 1/2 (idx=0/1) signal's negative overshoot value.
osc.channels[idx].rise Read (s) Read Channel 1/2 (idx=0/1) signal's rise time value.
osc.channels[idx].fall Read (s) Read Channel 1/2 (idx=0/1) signal's fall time value.
osc.channels[idx].pos_width Read (s) Read Channel 1/2 (idx=0/1) signal's positive width value.
osc.channels[idx].neg_width Read (s) Read Channel 1/2 (idx=0/1) signal's negative width value.
osc.channels[idx].pos_duty Read (s) Read Channel 1/2 (idx=0/1) signal's positive duty cycle value.
osc.channels[idx].neg_duty Read (s) Read Channel 1/2 (idx=0/1) signal's negative duty cycle value.
osc.time_base Read/Write 0.0000001 - 1 (s) Set Oscilloscope time base.
osc.time_position Read/Write (-5) - 5 (s) Set Oscilloscope time position.
osc.measure_all Read/Write true(on); false(off) Enable/Disable Display All Measurements.
osc.measure Read/Write true(on); false(off) Enable/Disable Measure Feature .
osc.measure_all Read/Write true(on); false(off) Enable/Disable Display All Measurements.
osc.counter Read/Write true(on); false(off) Enable/Disable Counter feature for Measurements.
osc.statistics Read/Write true(on); false(off) Enable/Disable Statistics feature for Measurements.
osc.cursors Read/Write true(on); false(off) Enable/Disable Cursors on plot.
osc.horizontal_cursors Read/Write true(on); false(off) Enable/Disable Horizontal Cursors on plot.
osc.vertical_cursors Read/Write true(on); false(off) Enable/Disable Vertical Cursors on plot.
osc.cursors_position Read/Write 0-3 Set Cursors Table position on plot.
osc.cursors_transparency Read/Write 0-100 (%) Set Cursors Table transparency on plot.
osc.auto_trigger Read/Write true(auto); false(normal) Set Trigger mode to Auto/Normal.
osc.internal_trigger Read/Write true(on); false(off) Enable/Disable Internal Trigger.
osc.external_trigger Read/Write true(on); false(off) Enable/Disable External Trigger.
osc.trigger_source Read/Write 0;1 Select Channel 1/2 (0/1) as Trigger Source.
osc.trigger_level Read/Write (-25) - 25 (V) Set Trigger Level.
osc.trigger_hysteresis Read/Write 0 - 2.5 (V) Set Trigger Hysteresis.
osc.running Read/Write true(on);false(off) Run Oscilloscope instrument.

Pattern Generator

Command Permission Values Description
pattern.running Read/Write true(on);false(off) Run Pattern Generator instrument.

Logic Analyzer

Command Permission Values Description
logic.running Read/Write true(on);false(off) Run Logic Analyzer instrument.

Spectrum Analyzer

Command Permission Values Description
spectrum.running Read/Write true(on);false(off) Run Spectrum Analyzer instrument.

Examples

List of script examples can be found here:

Resources

university/tools/m2k/scopy/scripting-guide.1544106596.txt.gz · Last modified: 06 Dec 2018 15:29 by Antoniu Miclaus