This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:tools:m2k:scopy:scripting-guide [08 Jun 2018 16:40] – add examples Antoniu Miclaus | university:tools:m2k:scopy:scripting-guide [06 Dec 2018 15:29] – Antoniu Miclaus | ||
---|---|---|---|
Line 11: | Line 11: | ||
The scripts can be run in two different ways: | The scripts can be run in two different ways: | ||
- | === Via command line: === | + | ==== Via command line: ==== |
< | < | ||
Line 17: | Line 17: | ||
</ | </ | ||
- | === Via Debugger Instrument === | + | ==== Via Debugger Instrument |
- | To open the Debugger in Scopy tool, its visibility must be enbled in the Instrument Menu. To do this, open the Scopy.ini file under the following path: " | + | To open the Debugger in Scopy tool, its visibility must be enbled in the Instrument Menu. To do this, open the Scopy.ini file under the following path: " |
<WRAP centeralign> | <WRAP centeralign> | ||
</ | </ | ||
+ | |||
+ | Now open Scopy: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
Line 56: | Line 58: | ||
| dio.dir[idx] | | dio.dir[idx] | ||
| dio.out[idx] | | dio.out[idx] | ||
- | | dio.gpi[idx] | + | | dio.gpi[idx] |
| dio.running | | dio.running | ||
Line 201: | Line 203: | ||
===== Examples ===== | ===== Examples ===== | ||
- | List of script examples: | + | List of script examples |
+ | |||
+ | * [[https:// | ||
- | * {{ : | + | ===== Resources ===== |
- | * {{ :university: | + | * [[https://wiki.qt.io/ |
- | * {{ : | + | |
+ | **Return to [[university: |