This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:scopy:power-supply [19 Jun 2017 10:33] – update info Antoniu Miclaus | university:tools:m2k:scopy:power-supply [07 Apr 2021 22:09] (current) – adding video Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Scopy Power Supply ====== | ====== Scopy Power Supply ====== | ||
+ | |||
+ | ===== Video ===== | ||
+ | {{youtube> | ||
===== Introduction ===== | ===== Introduction ===== | ||
- | The Power Supply instrument is the fourth | + | The Power Supply instrument is the last item in the Scopy instrument menu list, by default, displayed at the far left of the Scopy window. |
- | {{ : | + | {{: |
The small white squares to the right of the instrument names control the run/stop functions of the instruments, | The small white squares to the right of the instrument names control the run/stop functions of the instruments, | ||
- | {{ : | + | {{ : |
This instruments allows you to control the voltage output of the V+ (positive output) and V- (negative output) pins of the M2K. | This instruments allows you to control the voltage output of the V+ (positive output) and V- (negative output) pins of the M2K. | ||
Line 25: | Line 28: | ||
=== Independent Controls === | === Independent Controls === | ||
- | {{ : | + | {{ : |
By selecting the " | By selecting the " | ||
When enabled, the Enabled green buttons will turn into Disable red/orange buttons. Then, the corresponding output is active, until the Disable button is clicked again. | When enabled, the Enabled green buttons will turn into Disable red/orange buttons. Then, the corresponding output is active, until the Disable button is clicked again. | ||
+ | \\ | ||
+ | \\ | ||
=== Tracking === | === Tracking === | ||
- | {{ : | + | {{ : |
The " | The " | ||
In this mode, the Enable button of the negative output channel is disabled; the channel is enabled and disabled dynamically at the same time as the positive channel. | In this mode, the Enable button of the negative output channel is disabled; the channel is enabled and disabled dynamically at the same time as the positive channel. | ||
+ | \\ | ||
+ | \\ | ||
==== Positive/ | ==== Positive/ | ||
- | {{ : | + | {{ : |
In the “Positive output” control, the output can be set from 0 to 5 V, whereas, in the Negative output control, the output can be set from -5 to 0 V. You can select units for the value, Volts or mVolts. You can either input the value directly or use the +/- control to change the voltage output value. | In the “Positive output” control, the output can be set from 0 to 5 V, whereas, in the Negative output control, the output can be set from -5 to 0 V. You can select units for the value, Volts or mVolts. You can either input the value directly or use the +/- control to change the voltage output value. | ||
The increment/ | The increment/ | ||
The default increment/ | The default increment/ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | |||
+ | **Return to [[university: |