Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:tools:m2k:scopy:plugins:swiot1l [25 Aug 2023 11:12] – add macos installer Alexandra Trifanuniversity:tools:m2k:scopy:plugins:swiot1l [22 Nov 2023 10:37] (current) – don't update the installer for macos due to some dmg issues Alexandra Trifan
Line 12: Line 12:
 <WRAP round download> <WRAP round download>
 **Scopy for Windows ** **Scopy for Windows **
-  * Download: [[https://swdownloads.analog.com/cse/ad-swiot1l-sl/scopy-prealpha-swiot1l/scopy-prealpha-windows-setup.zip| Installer for latest release (Windows 64/32-bit)]]+  * Download: [[https://swdownloads.analog.com/cse/ad-swiot1l-sl/scopy-alpha-swiot1l/scopy-alpha-windows-setup.zip| Installer for latest release (Windows 64/32-bit); Updated: November 2023]]
  
 **Scopy for Windows portable ** **Scopy for Windows portable **
-  * Download: [[https://swdownloads.analog.com/cse/ad-swiot1l-sl/scopy-prealpha-swiot1l/scopy-prealpha-windows-portable.zip| Portable version for latest release (Windows 64/32-bit)]]+  * Download: [[https://swdownloads.analog.com/cse/ad-swiot1l-sl/scopy-alpha-swiot1l/scopy-alpha-windows-portable.zip| Portable version for latest release (Windows 64/32-bit); Updated: November 2023]]
  
 **Scopy for Linux ** **Scopy for Linux **
-  * Download: [[https://swdownloads.analog.com/cse/ad-swiot1l-sl/scopy-prealpha-swiot1l/scopy-prealpha-linux.zip| Scopy Flatpak installer]]+  * Download: [[https://swdownloads.analog.com/cse/ad-swiot1l-sl/scopy-alpha-swiot1l/scopy-alpha-linux.zip| Scopy Flatpak installer; Updated: November 2023]]
  
 **Scopy for OSX ** **Scopy for OSX **
Line 48: Line 48:
 Scopy is able to control and operate multiple devices. In order to use it for the AD-SWIOT1L-SL system, the user should click the "Add Device"(+) button displayed on the front page of the application. Scopy is able to control and operate multiple devices. In order to use it for the AD-SWIOT1L-SL system, the user should click the "Add Device"(+) button displayed on the front page of the application.
  
-The video attached above demonstrates the process of connecting to the board. First it will scan the network in order to detect the device. If the device is connected to the network and able to be scanned, it will appear in the list as **ip:swiot.local**. If the device is not available in the list, but the IP is known, the user can manually write the IP in the URI textbox and proceed forward.+The video attached above demonstrates the process of connecting to the board. First it will scan the network in order to detect the device. If the device is connected to the network and able to be scanned, it will appear in the list as **ip:analog.local**. If the device is not available in the list, but the IP is known, the user can manually write the IP in the URI textbox and proceed forward. The default static IP for all the boards is **169.254.97.40** .
  
 Once found and verified Scopy will present a list of compatible instruments. The list of instruments is explained below, but during this step the user can enable or disable Scopy functionalities for this board.  Once found and verified Scopy will present a list of compatible instruments. The list of instruments is explained below, but during this step the user can enable or disable Scopy functionalities for this board. 
university/tools/m2k/scopy/plugins/swiot1l.txt · Last modified: 22 Nov 2023 10:37 by Alexandra Trifan