The Scopy AD-SWIOT1L-SL plugin is responsible with the operation and control of the AD-SWIOT1L-SL platform.
The Scopy AD-SWIOT1L-SL plugin, while based on the Scopy application infrastructure, is tailored to provide all the specific functionalities of this system.
Scopy for Windows
Scopy for Windows portable
Scopy for Linux
Scopy for OSX
Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required.
Setup Flatpak using this setup guide for your Linux distribution.
After Flatpak is setup get the Scopy.flatpak file from the downloaded archive and run:
flatpak install scopy--flatpak.flatpak
Double click the downloaded .dmg to make its content available. “Scopy” will show up in the Finder sidebar and a window showing the content should open up.
Drag the application from the .dmg window into Applications to install and wait for the process to finish.
Scopy is able to control and operate multiple devices. In order to use it for the AD-SWIOT1L-SL system, the user should click the “Add Device”(+) button displayed on the front page of the application.
The video attached above demonstrates the process of connecting to the board. First it will scan the network in order to detect the device. If the device is connected to the network and able to be scanned, it will appear in the list as ip:swiot.local. If the device is not available in the list, but the IP is known, the user can manually write the IP in the URI textbox and proceed forward.
Once found and verified Scopy will present a list of compatible instruments. The list of instruments is explained below, but during this step the user can enable or disable Scopy functionalities for this board.
Going forward the homepage of the board is displayed. The homepage displays some basic information about the board, including its network IP. It also contains three buttons. One will perform the connection to the device, the second one performs identification and will blink a led on the board and the third one will start a quick tutorial for Scopy first time users. The tutorial is recommended in addition to this user guide as it will highlight and explain the user interface controls for the SWIOT1L available instruments.
This warning may appear in any of the instruments that interact with AD-SWIOT1L-SL. The user should check the external power supply switch position and verify which option is used to power the system.
More details on switching through the board states are provided on specific instrument documentation.