This is an old revision of the document!
Install a Qt 5 version (>5.12) using an online or offline installer from the official Qt downloads page.
Install dependencies
git clone https://github.com/analogdevicesinc/scopy.gitThis will fetch the latest sources from GitHub to a “scopy” directory.
In order to install the dependencies run the following script:
scopy/CI/appveyor/install_ubuntu_deps.shThis should install all of the dependencies required to build Scopy.
cd scopy mkdir build && cd build cmake -DCMAKE_PREFIX_PATH=/home/adi/Qt/5.15.0/gcc_64/lib/cmake ../Where -DCMAKE_PREFIX_PATH=path to the installed Qt version If everything goes well, the output should be “Configuring done” and “Generating done”.
Now build the project:
makeAnd run Scopy:
./scopy
Alternatively you can open QtCreator from the Qt folder. Open, configure and build the project.
Return to Scopy Main Page