This is an old revision of the document!
Install Qt 5 using an online or offline installer from the official Qt downloads page.
Install git, cmake, libzip, autoconf, libtool and libxml
sudo apt-get install git cmake libzip-dev autoconf libtool libxml2 libxml2-dev
Build and install Boost
cd ~ wget https://netcologne.dl.sourceforge.net/project/boost/boost/1.63.0/boost_1_63_0.tar.gz tar -xzvf boost_1_63_0.tar.gz cd boost_1_63_0 ./bootstrap.sh --with-libraries=date_time,filesystem,program_options,regex,system,test,thread ./b2 sudo ./b2 install
Build and install Markdown
cd ~ wget https://pypi.python.org/packages/1d/25/3f6d2cb31ec42ca5bd3bfbea99b63892b735d76e26f20dd2dcc34ffe4f0d/Markdown-2.6.8.tar.gz tar -xzvf Markdown-2.6.8.tar.gz cd Markdown-2.6.8 ./setup.py build sudo ./setup.py install
Install Python header files
sudo apt-get install python-dev sudo apt-get install python3-dev
Build and install Cheetah
cd ~ wget https://pypi.python.org/packages/cd/b0/c2d700252fc251e91c08639ff41a8a5203b627f4e0a2ae18a6b662ab32ea/Cheetah-2.4.4.tar.gz tar -xzvf Cheetah-2.4.4.tar.gz cd Cheetah-2.4.4 ./setup.py build sudo ./setup.py install
Install libfftw3
sudo apt-get install libfftw3-dev
Build and install Volk
cd ~ wget http://libvolk.org/releases/volk-1.3.tar.gz tar -xzvf volk-1.3.tar.gz cd volk-1.3 mkdir build && cd build cmake .. make sudo make install
Build and install GNU Radio
cd ~ git clone https://github.com/gnuradio/gnuradio cd gnuradio mkdir build && cd build cmake -DENABLE_INTERNAL_VOLK:BOOL=OFF -DENABLE_GR_FEC:BOOL=OFF -DENABLE_GR_DIGITAL:BOOL=OFF -DENABLE_GR_DTV:BOOL=OFF -DENABLE_GR_ATSC:BOOL=OFF -DENABLE_GR_AUDIO:BOOL=OFF -DENABLE_GR_CHANNELS:BOOL=OFF -DENABLE_GR_NOAA:BOOL=OFF -DENABLE_GR_PAGER:BOOL=OFF -DENABLE_GR_TRELLIS:BOOL=OFF -DENABLE_GR_VOCODER:BOOL=OFF .. make sudo make install
Install libffi, libmount, libpcre, libglib, libsigc++, libglibmm, doxygen
sudo apt-get install libffi-dev libmount-dev libpcre3-dev libglib2.0-dev libsigc++-2.0-dev libglibmm-2.4-dev doxygen
Build and install libsigrok
cd ~ git clone https://github.com/sschnelle/libsigrok/ cd libsigrok ./autogen.sh ./configure --disable-all-drivers --enable-bindings --enable-cxx make sudo make install
Build and install libsigrokdecode
cd ~ wget http://sigrok.org/download/source/libsigrokdecode/libsigrokdecode-0.4.1.tar.gz tar -xzvf libsigrokdecode-0.4.1.tar.gz cd libsigrokdecode-0.4.1 ./configure make sudo make install
Install OpenGL development files
sudo apt-get install libglu1-mesa-dev
Install curl
sudo apt-get install curl
Build and install Qwt
Before building Qwt, you need to check out your version of qmake.
Depending on the location of your Qt installation, the output of the following command can be either the version of Qt or an error.
qmake --version
If the output is an error it means you have a custom location for Qt. Please use the full path of qmake 5 in the following steps.
Example:
Use /opt/Qt/5.9.1/gcc_64/bin/qmake instead of qmake
If the Qt version is less than 5, you can do the following:
export QT_SELECT=5
Now we can build and install Qwt:
cd ~ git clone https://github.com/osakared/qwt cd qwt git checkout qwt-6.1-multiaxes gedit qwtconfig.pri
Change QWT_INSTALL_PREFIX to /usr/local
qmake qwt.pro make sudo make install
Build and install Qwt Polar
cd ~ wget https://downloads.sourceforge.net/project/qwtpolar/qwtpolar/1.1.1/qwtpolar-1.1.1.tar.bz2 tar xvjf qwtpolar-1.1.1.tar.bz2 cd qwtpolar-1.1.1 curl -o qwtpolar-qwt-6.1-compat.patch https://raw.githubusercontent.com/analogdevicesinc/scopy-flatpak/master/qwtpolar-qwt-6.1-compat.patch patch -p1 < qwtpolar-qwt-6.1-compat.patch gedit qwtpolarconfig.pri
Change QWT_POLAR_INSTALL_PREFIX to /usr/local and remove the line:
QWT_POLAR_CONFIG += QwtPolarExamples
qmake qwtpolar.pro make sudo make install
Install libusb
sudo apt-get install libusb-1.0-0-dev
Build and install libiio
cd ~ git clone https://github.com/analogdevicesinc/libiio cd libiio && mkdir build && cd build cmake -DCMAKE_INSTALL_LIBDIR:STRING=lib -DINSTALL_UDEV_RULE:BOOL=OFF -DWITH_TESTS:BOOL=OFF -DWITH_DOC:BOOL=OFF -DWITH_IIOD:BOOL=OFF -DWITH_LOCAL_BACKEND:BOOL=OFF -DWITH_MATLAB_BINDINGS_API:BOOL=OFF .. make sudo make install
Install flex
sudo apt-get install flex
Install bison
sudo apt-get install bison
Install libad9361
cd ~ git clone https://github.com/analogdevicesinc/libad9361-iio cd libad9361-iio mkdir build && cd build cmake .. make sudo make install
Build and install the IIO blocks for GNU Radio
cd ~ git clone https://github.com/analogdevicesinc/gr-iio cd gr-iio mkdir build && cd build cmake .. make sudo make install
git clone https://github.com/analogdevicesinc/scopy.gitThis will fetch the latest sources from GitHub to a “scopy” directory.
cd scopy mkdir build && cd build cmake ..If everything goes well, the output should be “Configuring done” and “Generating done”.
Now build the project:
makeAnd run Scopy:
./scopy
Return to Scopy Main Page