This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:scopy:build-linux [22 Jul 2020 13:55] – Update Linux build guide Adrian Suciu | university:tools:m2k:scopy:build-linux [24 Jul 2020 10:54] (current) – Updated Linux build guide Adrian Suciu | ||
---|---|---|---|
Line 13: | Line 13: | ||
This will fetch the latest sources from GitHub to a " | This will fetch the latest sources from GitHub to a " | ||
- | In order to install the dependencies run the following | + | This following |
- | Replace QMAKE=... from scopy/ | + | |
< | < | ||
**scopy/ | **scopy/ | ||
</ | </ | ||
+ | or if you want to use a custom version of Qt (the one you just installed) - scopy/ | ||
+ | < | ||
+ | **scopy/ | ||
+ | | ||
+ | </ | ||
+ | |||
This should install all of the dependencies required to build Scopy. | This should install all of the dependencies required to build Scopy. | ||
===== Building Scopy ===== | ===== Building Scopy ===== | ||
- | + | If you are using a custom Qt version set -DCMAKE_PREFIX_PATH to the <Qt installation folder>/ | |
< | < | ||
**cd scopy | **cd scopy | ||
Line 30: | Line 33: | ||
cmake -DCMAKE_PREFIX_PATH=/ | cmake -DCMAKE_PREFIX_PATH=/ | ||
</ | </ | ||
- | Where -DCMAKE_PREFIX_PATH=path to the installed Qt version | ||
If everything goes well, the output should be " | If everything goes well, the output should be " | ||