Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
university:tools:m2k:scopy-troubleshooting [04 Feb 2022 13:55] Adrian Suciuuniversity:tools:m2k:scopy-troubleshooting [16 Feb 2022 10:08] – [Reinstall & INI files] Adrian Suciu
Line 11: Line 11:
  
 ===== Reinstall & INI files ===== ===== Reinstall & INI files =====
- 
-Scopy configuration can sometimes get messed up when updating as opposed to uninstall/reinstall. If you are facing this issue, you can try uninstalling Scopy and then reinstall.  
-<note important> Make sure that after uninstall Scopy's folder is clear</note> 
-Make sure you install Scopy in a location that doesn't require any write privileges since Scopy needs to write to it's installation folder. 
-  
 ''Scopy.ini'' and ''Preferences.ini'' contain the user-settings that are saved in-between sessions. Sometimes these can get messed up and can cause problems. In order to reset them, go to: ''Scopy.ini'' and ''Preferences.ini'' contain the user-settings that are saved in-between sessions. Sometimes these can get messed up and can cause problems. In order to reset them, go to:
 These file are located in: These file are located in:
Line 23: Line 18:
  
 and delete (or rename) ''Scopy.ini'', ''Scopy.ini.bak'', ''Preferences.ini'', ''Preferences.ini.bak''. The preference is to rename things with a different suffix, so if you need to report a bug, the file still exists. and delete (or rename) ''Scopy.ini'', ''Scopy.ini.bak'', ''Preferences.ini'', ''Preferences.ini.bak''. The preference is to rename things with a different suffix, so if you need to report a bug, the file still exists.
 +
 +Scopy configuration can sometimes get messed up when updating as opposed to uninstall/reinstall. If you are facing this issue, you can try uninstalling Scopy and then reinstall. 
 +<note important> Make sure that after uninstall Scopy's folder is clear</note>
 +Make sure you install Scopy in a location that doesn't require any write privileges since Scopy needs to write to it's installation folder.
 + 
 +
  
 ===== Connecting through the network interface ===== ===== Connecting through the network interface =====
university/tools/m2k/scopy-troubleshooting.txt · Last modified: 15 Mar 2024 10:26 by Alexandra Trifan