Scopy.ini and Preferences.ini contain the user-settings that are saved in-between sessions. Sometimes these can get messed up and can cause problems. In order to reset them, go to:
Windows: C:\Users\your_username\AppData\Roaming\ADI
Linux: /home/user/.config/ADI
Mac: /Users/user/.config/analog.com
and delete Scopy.ini, Scopy.ini.bak, Preferences.ini, Preferences.ini.bak
If you are having trouble connecting through USB, you can always connect to the ADALM2000 through the network interface. The USB connection can cause all kinds of problems on various systems. In order to connect through the emulated network interface run these steps here
https://wiki.analog.com/university/tools/m2k/scopy?s[]=remote#connecting_to_a_remote_device
Visit the ADALM2000 firmware page https://github.com/analogdevicesinc/m2k-fw/releases.
Compare the latest firmware version on this page with the one you have installed. Follow these steps to update the firmware: https://wiki.analog.com/university/tools/m2k/common/firmware
Download latest version of https://github.com/analogdevicesinc/libiio/releases .
Open a command prompt and run
iio_info -a
or
iio_info -u "ip:192.168.2.1"