Wiki

This version (31 Dec 2020 07:23) was approved by Robin Getz.The Previously approved version (05 Nov 2020 17:14) is available.Diff

Scopy

About

Scopy is a multi-functional software toolset with strong capabilities for signal analysis. If you are interested in some screen shots

Download

In order to have Scopy working with ADALM2000 please make sure that the Device Drivers are installed. A guide on this topic can be found in the section:

Installation

Scopy for Windows

Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required.

Video


Scopy for Linux

Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using this setup guide for your Linux distribution.

For Ubuntu, you can use the following steps:

    sudo add-apt-repository ppa:alexlarsson/flatpak
    sudo apt update
    sudo apt install flatpak
    flatpak remote-add --if-not-exists flathub https://flathub.org/repo/flathub.flatpakrepo

After this, get the Scopy.flatpak file from the downloaded archive and run:

    flatpak install scopy-v1.1.1-Linux-flatpak.flatpak

Video


Scopy for OSX

Double click the downloaded .dmg to make its content available. “Scopy” will show up in the Finder sidebar and a window showing the content should open up.
Drag the application from the .dmg window into Applications to install and wait for the process to finish.

Video

Launching

Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder.

On Linux, you can also run it using:

    flatpak run org.adi.Scopy

Using the Application

Home

The Home view is divided into four sections:

  • Devices(1): List of devices (USB or remote) that Scopy can connect to. USB devices are detected automatically at startup. The Add button can be used to add remote devices to the list.
  • Instruments Menu(2): List with instruments provided by the application.
  • Information Window(3): Section containing the welcome, add device page and for each device a description.
  • General Settings Menu(4): Save and load session and the preferences menu.

Scopy Home View

Connecting to a USB device

If a compatible USB device is available it will be displayed in the Devices section.

To connect to that device click on the device and then click the Connect button in the Information Window.

If the connection was established, the device will have a green status line under it and you will be able to disconnect from it in the same Information Window.

Scopy Home View

Connecting to a remote device

To connect to a remote device click on the Plus icon. Enter the IP of the remote device into the Hostname field and click the Connect button. If a device can be detected at the IP you provided, the Connect button will change to an Add button and you can click on it to add the remote device to the list of detected devices.

Clicking the Forget Device button will remove the device from the list. Clicking the Identify button will make the device blink.


General Settings Menu

The save/load buttons can be used to save the current session or load another session. The preferences button will open the preferences for Scopy where different options for different tools can be modified.

Clicking the Reset Scopy button will reset the application to a default configuration.

Checking the user notes preference will enable a tool where the user can add different pages with html formatted text


User Guides

Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, a list of instruments that are available for that device will be enabled. Each instrument can be opened from the left menu. The icon on the right of the instrument name specifies that the instrument is enabled and provides a shortcut that allows an instrument to be turned on or off.

The instruments menu can be minimized by clicking on the Scopy button near the top-left window.

 Scopy Minimized Menu View

Detaching Instruments

Scopy provides the detaching into multiple windows feature for each instrument available, providing a better view/manipulation.

There are 2 ways to do this:

  1. Drag and Drop - select the desired instrument drag it outside Instrument Menu section and drop it inside the application window area.

 Scopy Drag and Drop

  1. Double Click - first make sure that the Double click to detach a tool option is enabled in the Preferences menu; double-click on the desired instrument to detach it.

 Scopy Double Click Detach


Instruments Overview

Scripts

User guide on how to use scripts with Scopy:


Building

Complete Scopy build guides on:


Source code

The source code for the entire application can be found on github.

university/tools/m2k/scopy.txt · Last modified: 31 Dec 2020 07:23 by Robin Getz