Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
university:tools:m2k:matlab [15 Jul 2020 22:17] – Minor tweaks Travis Collins | university:tools:m2k:matlab [14 Jan 2021 05:38] – use ez> mw> wiki interwiki links Robin Getz |
---|
====== Quick Start ====== | ====== Quick Start ====== |
| |
To get started with libm2k+MATLAB there are integrated installers available for [[https://www.mathworks.com/matlabcentral/fileexchange/74385-libm2k-matlab|Windows]]. Simply download the MLTBX file and open it within MATLAB. This will install the necessary libraries and classes to interface with M2K. The Windows installer packages the dependent libraries libiio, libm2k, and the MATLAB bindings so they do not need to be installed externally. The only requirement is the [[https://wiki.analog.com/university/tools/pluto/drivers/windows|M2K driver]]. For Linux support see the [[#Linux Support|section below]]. | To get started with libm2k+MATLAB there are integrated installers available for [[mw>matlabcentral/fileexchange/74385-libm2k-matlab|Windows]]. Simply download the MLTBX file and open it within MATLAB. This will install the necessary libraries and classes to interface with M2K. The Windows installer packages the dependent libraries libiio, libm2k, and the MATLAB bindings so they do not need to be installed externally. The only requirement is the [[/university/tools/pluto/drivers/windows|M2K driver]]. For Linux support see the [[#Linux Support|section below]]. |
| |
After installation of the driver and the MLTBX file, you will have access to the bindings through [[mw>help/matlab/call-cpp-library-functions.html|MATLAB's clib interface for C++ libraries]]. For libm2k this will be in the form:<code>clib.libm2k.libm2k.<M2K classes> </code> | After installation of the driver and the MLTBX file, you will have access to the bindings through [[mw>help/matlab/call-cpp-library-functions.html|MATLAB's clib interface for C++ libraries]]. For libm2k this will be in the form:<code>clib.libm2k.libm2k.<M2K classes> </code> |
====== Support ====== | ====== Support ====== |
| |
For support questions please post them on EngineerZone under the [[https://ez.analog.com/adieducation/university-program|Virtual Classroom Forum]]. | For support questions please post them on EngineerZone under the [[ez>adieducation/university-program|Virtual Classroom Forum]]. |
| |
If you find any bugs please report them on the [[https://github.com/analogdevicesinc/libm2k/issues|libm2k issues tracker on GitHub]]. | If you find any bugs please report them on the [[https://github.com/analogdevicesinc/libm2k/issues|libm2k issues tracker on GitHub]]. |
| |