Wiki

This version is outdated by a newer approved version.DiffThis version (11 Jul 2018 15:38) was approved by Antoniu Miclaus.

This is an old revision of the document!


ADALM2000 for Developers

The people who typical read these pages are those who write custom software or HDL (for the FPGA) that run directly on the M2K device. This may put the M2K in different modes, and support different external USB devices (including USB/LAB, or USB/WiFi), extending the capabilities of the device, or completely changing the data that is transferred to the host. Since the goal of the project is to keep things as open as possible, the details on how to compile kernels, create bit files, assemble FIT files and load them into the device, should be found here.

While we do have a few examples, and show how to re-create the default software loads, since this the hardware can be nearly a blank slate for your project, you can do anything you want.

Content

university/tools/m2k/developers.1531316324.txt.gz · Last modified: 11 Jul 2018 15:38 by Antoniu Miclaus