Wiki

This version (07 Apr 2021 14:52) was approved by Cristina Suteu.The Previously approved version (20 Jan 2020 12:45) is available.Diff

ADALM2000 for Developers

The people who typical read these pages are those who write custom software or HDL (for the FPGA) that run directly on the M2K device. This may put the M2K in different modes, and support different external USB devices (including USB/LAB, or USB/WiFi), extending the capabilities of the device, or completely changing the data that is transferred to the host. Since the goal of the project is to keep things as open as possible, the details on how to compile kernels, create bit files, assemble FIT files and load them into the device, should be found here.

While we do have a few examples, and show how to re-create the default software loads, since this the hardware can be nearly a blank slate for your project, you can do anything you want.

Content

please make sure that all these are in the ./devs subdirectory

  1. Introduction (Coming soon)
  2. Hardware
    1. Detailed Specifications (Coming soon)
    2. Detailed Performance (Coming soon)
    3. Accessing the Console(Coming soon) with the ADALM-JTAGUART adapter
    4. Accessing FPGA JTAG(Coming soon) with the ADALM-JTAGUART adapter
  3. Device Drivers
    1. AXI DMAC Linux Driver
    2. etc.
  4. Building the Firmware image from source
university/tools/m2k/developers.txt · Last modified: 07 Apr 2021 14:52 by Cristina Suteu