This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:tools:m2k:common:firmware [13 Jun 2020 02:32] – [Entering DFU mode] Robin Getz | university:tools:m2k:common:firmware [29 Jan 2021 20:12] – [Entering DFU mode] - fix links Robin Getz | ||
---|---|---|---|
Line 62: | Line 62: | ||
- From the device linux console type **'' | - From the device linux console type **'' | ||
- The USB console USB CDC ACM aka. ttyACM0 using putty, minicom, tera Term, etc. | - The USB console USB CDC ACM aka. ttyACM0 using putty, minicom, tera Term, etc. | ||
- | - The UART console using [[university:tools:jtaguart|ADALM-JTAGUART]]. | + | - The UART console using [[university/tools/uartjtag|ADALM-JTAGUART]]. |
- The network console using ssh/slogin. | - The network console using ssh/slogin. | ||
- | - Directly from u-boot serial console type: **run dfu_sf**. Access to the uboot command console is only available using [[university:tools:jtaguart|ADALM-JTAGUART]] | + | - Directly from u-boot serial console type: **run dfu_sf**. Access to the uboot command console is only available using [[university/tools/uartjtag|ADALM-JTAGUART]] |
=== When does the device automatically enter DFU mode? === | === When does the device automatically enter DFU mode? === |