This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:tools:m2k:alice:users-guide-m2k [10 Mar 2021 13:50] – [The Right Side Menu Section] Doug Mercer | university:tools:m2k:alice:users-guide-m2k [10 Mar 2021 19:25] (current) – move important notice to very top of page Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
======Active Learning Interface (for) Circuits (and) Electronics for M2K: ====== | ======Active Learning Interface (for) Circuits (and) Electronics for M2K: ====== | ||
+ | |||
+ | <note important> | ||
=====Objective: | =====Objective: | ||
Line 29: | Line 31: | ||
The ALICE 2.0 Desktop program for the ALM2000 is written in Python and if run from the source code requires version 2.7.8 or greater of Python be installed on the user’s computer. The program only imports modules generally included with standard Python installation packages. | The ALICE 2.0 Desktop program for the ALM2000 is written in Python and if run from the source code requires version 2.7.8 or greater of Python be installed on the user’s computer. The program only imports modules generally included with standard Python installation packages. | ||
- | |||
- | <note important> | ||
====Windows: | ====Windows: |