Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
university:tools:m2k:accessories:power [23 Jul 2021 15:19] – [Description] Pop Andreeauniversity:tools:m2k:accessories:power [27 Aug 2021 14:01] – Replaced pictures Pop Andreea
Line 3: Line 3:
 The AD-M2KPWR-EBZ is an ADALM2000 add-on board which increases the output current capability up to 700mA. This board can be also used as a standalone benchtop power supply with positive and negative outputs. The AD-M2KPWR-EBZ is an ADALM2000 add-on board which increases the output current capability up to 700mA. This board can be also used as a standalone benchtop power supply with positive and negative outputs.
  
-{{:university:tools:m2k:accessories:pwr_b.png?400|}} 
  
-Figure 1. AD-M2KPWR-EBZ Top view +{{:university:tools:m2k:accessories:ad-m2kpwr-ebztop.jpg?500|}} 
 +{{:university:tools:m2k:accessories:ad-m2kpwr-ebzbottom.jpg?500|}} 
 + 
 +Figure 1. AD-M2KPWR-EBZ Top view and bottom view
 ===== Features ===== ===== Features =====
   * ADALM2000 compatible   * ADALM2000 compatible
Line 40: Line 42:
   * Standoffs and screws   * Standoffs and screws
  
-{{:university:tools:m2k:accessories:pwr_a.png?400|}}+ 
 +{{:university:tools:m2k:accessories:ad-m2kpwr-ebzangle.jpg?400|}} 
  
 Figure 2. AD-M2KPWR-EBZ Isometric view - Package contents Figure 2. AD-M2KPWR-EBZ Isometric view - Package contents
Line 46: Line 50:
 AD-M2KPWR-EBZ  must be supplied either from a 5.1V 3A USB Type C power adapter or from a lab supply using the screw terminal connector. Make sure that the jumper on the P2 connector is on the position corresponding to the chosen supply: AD-M2KPWR-EBZ  must be supplied either from a 5.1V 3A USB Type C power adapter or from a lab supply using the screw terminal connector. Make sure that the jumper on the P2 connector is on the position corresponding to the chosen supply:
  
- +<WRAP centeralign>{{:university:tools:m2k:accessories:vusbconn.png?600|}}</WRAP> 
-{{:university:tools:m2k:accessories:pwr_b_vusbvext_jumper.png?200|}} +<WRAP centeralign> Figure 3. AD-M2KPWR-EBZ supply select jumper</WRAP>
 ^ P2 ^ Selected supply method^  ^ P2 ^ Selected supply method^ 
 |Jumper 1-2 shorted | Vext - for external lab supply| |Jumper 1-2 shorted | Vext - for external lab supply|
 |Jumper 2-3 shorted | Vusb - for USB Type C power adapter| |Jumper 2-3 shorted | Vusb - for USB Type C power adapter|
  
 +
 +
 +<WRAP centeralign>{{:university:tools:m2k:accessories:20210615_1452544.jpg?600|}}</WRAP>
 +<WRAP centeralign> Figure 4.AD-M2KPWR-EBZ connected to ADALM2000 and USB Type C supply</WRAP>
  
 ====M2K and POT modes ==== ====M2K and POT modes ====
Line 58: Line 65:
 In M2K mode the board is plugged into ADALM2000. After that, the programable user supplies of ADALM2000 can be used as usual, but they will source more current. The jumper on the connector P7 must be in M2K- position and the jumper on the connector P6 must be in M2K+ position.  In M2K mode the board is plugged into ADALM2000. After that, the programable user supplies of ADALM2000 can be used as usual, but they will source more current. The jumper on the connector P7 must be in M2K- position and the jumper on the connector P6 must be in M2K+ position. 
  
-{{ :university:tools:m2k:accessories:20210615_145301.jpg?400 |}} 
  
-<WRAP centeralign> Figure 3. AD-M2KPWR-EBZ connected to ADALM2000 and USB Type C supply</WRAP>+<WRAP centeralign>  {{:university:tools:m2k:accessories:jumpers_mode_selection.png?600|}}</WRAP> 
 +<WRAP centeralign> Figure 5. AD-M2KPWR-EBZ POT/M2K mode setup jumpers</WRAP>
  
  
Line 74: Line 81:
 In POT mode the board can be used as a standalone benchtop power supply. The output voltage is adjusted with potentiometers R19 and R20. The output voltage will be available at the same pins: V+ and V-. In POT mode the board can be used as a standalone benchtop power supply. The output voltage is adjusted with potentiometers R19 and R20. The output voltage will be available at the same pins: V+ and V-.
  
-<WRAP centeralign> {{:university:tools:m2k:accessories:pwr_b_m2kpotjumpers.png?400|}}</WRAP> +
-<WRAP centeralign> Figure 4. AD-M2KPWR-EBZ POT/M2K mode setup jumpers</WRAP>+
  
  
university/tools/m2k/accessories/power.txt · Last modified: 05 May 2022 12:44 by Pop Andreea