Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
university:tools:m1k:firmware-upgrade [22 Oct 2020 16:06] – [Update using the smu executable] Robin Getz | university:tools:m1k:firmware-upgrade [08 Feb 2021 16:58] (current) – update links to libsmu wiki page Alexandra Trifan |
---|
==== Update using the smu executable ==== | ==== Update using the smu executable ==== |
| |
The ''smu'' executable (part of the [[https://github.com/analogdevicesinc/libsmu/releases/latest|libsmu]] package) provides some basic functionalities . In the following image you can see these functionalities and their corresponding call arguments: | The ''smu'' executable (part of the [[university:tools:m1k:libsmu|libsmu]] library) provides some basic functionalities . In the following image you can see these functionalities and their corresponding call arguments: |
<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> | <WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> |
<xterm> | <xterm> |