university:tools:m1k:analog-mux [29 Dec 2020 19:23]
Doug Mercer new analog accessory board version
university:tools:m1k:analog-mux [03 Jan 2021 22:21] (current)
Robin Getz fix links
Line 44: Line 44:
  
 <WRAP centeralign>​ Figure 8, Simply attach 74HC4052 on proto-board and jumper wires</​WRAP>​ <WRAP centeralign>​ Figure 8, Simply attach 74HC4052 on proto-board and jumper wires</​WRAP>​
 +
 +There are other analog multiplexer configurations in the generic CD4XXX series of CMOS ICs. The CD4051 is a single 8:1 mux and the CD4067 is a single 16:1 mux. The old Motorola MC14529B analog selector can be a configured as a dual 4-channel or single 8-channel device depending on how the input controls are used. By using 3 or all 4 of the digital PIO bits and two of these single multiplexers either 16 or even 32 signal channels could be measured. This [[https://​www.sparkfun.com/​products/​9056|16:​1 mux breakout board]] available from SparkFun is based on the CD74HC4067 and works well with the ALM1000. Another [[https://​www.sparkfun.com/​products/​13906|8 Channel Multiplexer Breakout]] based the 74HC4051 is also available.
  
 The SparkFun analog mux boards do not come with header connectors so they would need to be added. The pins on the connector do not line up with the M1k connectors so male to male jumpers would be needed as shown in the figure 9. The SparkFun analog mux boards do not come with header connectors so they would need to be added. The pins on the connector do not line up with the M1k connectors so male to male jumpers would be needed as shown in the figure 9.
Line 59: Line 61:
 There are other analog multiplexer configurations in the generic CD4XXX series of CMOS ICs. The CD4051 is a single 8:1 mux and the CD4067 is a single 16:1 mux. The old Motorola MC14529B analog selector can be a configured as a dual 4-channel or single 8-channel device depending on how the input controls are used. By using 3 or all 4 of the digital PIO bits and two of these single multiplexers either 16 or even 32 signal channels could be measured. These two mux breakout boards are available from SparkFun, the [[https://​www.sparkfun.com/​products/​9056|74HC4067 16:1 mux]] and the [[https://​www.sparkfun.com/​products/​13906|74HC4051 8:1 mux]]. Either works well with the ADALM1000. There are other analog multiplexer configurations in the generic CD4XXX series of CMOS ICs. The CD4051 is a single 8:1 mux and the CD4067 is a single 16:1 mux. The old Motorola MC14529B analog selector can be a configured as a dual 4-channel or single 8-channel device depending on how the input controls are used. By using 3 or all 4 of the digital PIO bits and two of these single multiplexers either 16 or even 32 signal channels could be measured. These two mux breakout boards are available from SparkFun, the [[https://​www.sparkfun.com/​products/​9056|74HC4067 16:1 mux]] and the [[https://​www.sparkfun.com/​products/​13906|74HC4051 8:1 mux]]. Either works well with the ADALM1000.
  
-Another functionally similar option is the [[http://​www.analog.com/​media/​en/​technical-documentation/​data-sheets/​ADG608_609.pdf|dual 4:1 ADG609]] and single ADG608 8:1 multiplexers,​ which have a different pin-out than the generic CD4051/52 multiplexers. Through-hole and surface mount ADG609 based boards similar to the one in figure 3 are also included in the zip file.+Another functionally similar option is the [[adi>media/​en/​technical-documentation/​data-sheets/​ADG608_609.pdf|dual 4:1 ADG609]] and single ADG608 8:1 multiplexers,​ which have a different pin-out than the generic CD4051/52 multiplexers. Through-hole and surface mount ADG609 based boards similar to the one in figure 3 are also included in the zip file.
  
 While the generic CD4052 is lower cost than the ADG609, there are two main advantages of using the ADG609 over the CD4052. The ADG609 on resistance maximum spec is 30 ohms, where the CD4052 on resistance maximum spec is 240 ohms and the 74HC4052 on resistance maximum spec is 120 ohms. This higher resistance could cause errors and distortions in the measurements under certain conditions. While the generic CD4052 is lower cost than the ADG609, there are two main advantages of using the ADG609 over the CD4052. The ADG609 on resistance maximum spec is 30 ohms, where the CD4052 on resistance maximum spec is 240 ohms and the 74HC4052 on resistance maximum spec is 120 ohms. This higher resistance could cause errors and distortions in the measurements under certain conditions.
university/tools/m1k/analog-mux.1609266181.txt.gz · Last modified: 29 Dec 2020 19:23 by Doug Mercer