This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:tools:alm1000-stripchart-users-guide [08 Mar 2016 17:03] – [Windows:] Doug Mercer | university:tools:m1k:alice:stripchart-users-guide [25 Mar 2016 18:15] – ↷ Links adapted because of a move operation Robin Getz | ||
---|---|---|---|
Line 7: | Line 7: | ||
=====Background: | =====Background: | ||
- | The ALM1000 contains two 16 bit 100KSPS analog to digital converters. These voltage inputs are often used to measure fast time varying waveforms as in the [[university: | + | The ALM1000 contains two 16 bit 100KSPS analog to digital converters. These voltage inputs are often used to measure fast time varying waveforms as in the [[university: |
=====Required files:===== | =====Required files:===== | ||
Line 28: | Line 28: | ||
It is assumed that the reader is somewhat familiar with the functionality and capabilities of the ADALM1000 hardware. For more on the ADALM1000 hardware please refer to the following documents: | It is assumed that the reader is somewhat familiar with the functionality and capabilities of the ADALM1000 hardware. For more on the ADALM1000 hardware please refer to the following documents: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
[[university: | [[university: | ||
[[university: | [[university: |