This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:alice-sa-1.0-users-guide [11 Aug 2015 02:28] – [Mode drop down menu] Doug Mercer | university:tools:m1k:alice:sa-users-guide [27 Jan 2021 23:01] (current) – use interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
======ALICE Spectrum Analyzer: | ======ALICE Spectrum Analyzer: | ||
+ | |||
+ | **This software uses an older version of libsmu / pysmu and is no longer recommended for use.** | ||
+ | |||
+ | [[university: | ||
+ | |||
=====Objective: | =====Objective: | ||
Line 11: | Line 16: | ||
All OS:\\ | All OS:\\ | ||
alice-SA-1.0.py(w)\\ | alice-SA-1.0.py(w)\\ | ||
- | adi_logo_alice.gif\\ | ||
{{: | {{: | ||
Windows:\\ | Windows:\\ | ||
- | [[https:// | + | [[https:// |
+ | |||
+ | Use of the [[university: | ||
Linux:\\ | Linux:\\ | ||
Line 33: | Line 39: | ||
[[university: | [[university: | ||
[[university: | [[university: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
=====Screen Setup:===== | =====Screen Setup:===== | ||
Line 67: | Line 73: | ||
====Curves drop down menu==== | ====Curves drop down menu==== | ||
- | The Curves button allows the selection of which signal waveforms will be displayed. The All button selects all four curves to be displayed and the None button clears all four curves. The Marker option turns on a text marker which displays the amplitude and frequency at the peak of the displayed signal. It is also possible to select which of the possible stored reference traces, if saved via the Store trace option, will be displayed. | + | The Curves button allows the selection of which signal waveforms will be displayed. The All button selects all four curves to be displayed and the None button clears all four curves. The Marker option turns on a text marker which displays the amplitude and frequency at the peak of the displayed signal. Options to display the difference ( subtraction ) of the CA-dBV – CB-dBV traces or the CB-dBV – CA-dBV traces. It is also possible to select which of the possible stored reference traces, if saved via the Store trace option, will be displayed. |
+ | |||
+ | The color of the CA-dBV and CB-dBV traces will turn red if the input signal goes beyond the 0 to +5 V analog input signal range. | ||
+ | |||
+ | ====PWR-ON==== | ||
+ | |||
+ | The green PWR-On button toggles on and off the fixed analog +2.5 V and +5 V power supplies. The button turns red when the supplies are off. The power supplies do not turn completely off but go to around +2 V and can supply only about 20 mA when shorted to ground. This is much less than the 200 mA or so they could supply if accidentally shorted when on. It is good practice to turn off the supplies ( or better yet disconnect ) when making any modifications to the circuit under test. | ||
====Run, Stop, Exit==== | ====Run, Stop, Exit==== | ||
Line 78: | Line 90: | ||
Load Config, commands for saving and loading configuration settings (.cfg file)\\ | Load Config, commands for saving and loading configuration settings (.cfg file)\\ | ||
Save Screen, command for saving the graphics display area to an encapsulated postscript file (.eps)\\ | Save Screen, command for saving the graphics display area to an encapsulated postscript file (.eps)\\ | ||
- | Save Data, command for saving the captured channel A and B amplitude vs frequency data to a coma separated values file (.csv) | + | Save Data, command for saving the captured channel A and B amplitude vs frequency data to a coma separated values file (.csv). The amplitude data can be saved as magnitude in Vrms ( type a 0 ) or in dBV ( type a 1 ). |
====Options drop down menu==== | ====Options drop down menu==== | ||
Smooth, an option to enabling smoothing where spline curves are used to connect the FFT frequency points rather than the default straight lines. | Smooth, an option to enabling smoothing where spline curves are used to connect the FFT frequency points rather than the default straight lines. | ||
+ | |||
+ | Cut-DC, an option that will remove the DC component from the sampled data record. It element by element subtracts the average value of the sample record. | ||
Store trace, no explanation required, you can store a reference trace with it. | Store trace, no explanation required, you can store a reference trace with it. | ||
+ | |||
Screen setup, to select the number of vertical divisions on the grid. Also for selecting smaller grids. Can be handy when you want to capture smaller spectrum analyzer bit map pictures for documentation or a website. | Screen setup, to select the number of vertical divisions on the grid. Also for selecting smaller grids. Can be handy when you want to capture smaller spectrum analyzer bit map pictures for documentation or a website. | ||
Line 116: | Line 131: | ||
The current low level ALM1000 software only outputs signals as single shot bursts when the analog signals ( voltage and current ) are being sampled. The Sync AWG check box must be checked if you want to produce outputs in sync with the analog trace sweeps. If you are in Hi-Z mode for both CH A and CH B and are using the ALM as just a 2 input spectrum analyzer the box should not be checked. | The current low level ALM1000 software only outputs signals as single shot bursts when the analog signals ( voltage and current ) are being sampled. The Sync AWG check box must be checked if you want to produce outputs in sync with the analog trace sweeps. If you are in Hi-Z mode for both CH A and CH B and are using the ALM as just a 2 input spectrum analyzer the box should not be checked. | ||
+ | |||
+ | The Sweep Gen drop down menu provides controls for generating frequency sweeps of the analog output sources. The screen traces are up-dated after each frequency step. It is best to select Peek Hold mode to display the amplitude response vs frequency. First is a radio button to select which output channel, or none will be swept. The selected output will be swept from the display Start Frequency to the Stop Frequency. The number of steps can be set using the Sweep Steps button. Lastly, there is a radio button selector for single or continuous sweep. The frequency sweep is started, or restarted from the beginning each time the Run button is pressed. | ||
The ALM hardware provides four 3.3V CMOS digital input / output pins. At this time only static hi low functionality is supported. A simple interface is provided here. The D Inp line displays the current state of any of the four pins configured as input as either [0] or [1] one for each pin, PIO 0, PIO 1, PIO, 2 and PIO 3 from left to right and are updated once each time the analog scope display is refreshed. The D Out line consists of four single digit entry fields, one for each pin, PIO 0, PIO 1, PIO, 2 and PIO 3 from left to right. An ' | The ALM hardware provides four 3.3V CMOS digital input / output pins. At this time only static hi low functionality is supported. A simple interface is provided here. The D Inp line displays the current state of any of the four pins configured as input as either [0] or [1] one for each pin, PIO 0, PIO 1, PIO, 2 and PIO 3 from left to right and are updated once each time the analog scope display is refreshed. The D Out line consists of four single digit entry fields, one for each pin, PIO 0, PIO 1, PIO, 2 and PIO 3 from left to right. An ' | ||
Line 121: | Line 138: | ||
At the bottom of this section, just above the ADI logo, are entry windows which allow input gain and offset correction for any external resistor divider attenuator networks that might be added to the channel A and B inputs ( possibly used when in the high impedance or Split I/O modes ). For more on the use of input attenuators please refer to the following two documents: | At the bottom of this section, just above the ADI logo, are entry windows which allow input gain and offset correction for any external resistor divider attenuator networks that might be added to the channel A and B inputs ( possibly used when in the high impedance or Split I/O modes ). For more on the use of input attenuators please refer to the following two documents: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
=====Frequency Analysis: | =====Frequency Analysis: | ||
Line 193: | Line 210: | ||
=====Examples: | =====Examples: | ||
+ | |||
+ | The following example shows a technique where ALICE-SA can be used to measure the amplitude vs frequency response of two simple RLC configurations. Shown in figure E1, first on the left is a parallel LC bandpass configuration and second on the right is a series LC bandstop configuration. Indicated by the green boxes are the connections to the ALM1000. Channel B is setup to output the driving function of the network. Channel A is setup as an input to measure the response seen across the LC network. For this example R< | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | In a linear system, the frequency response can be obtained by sweeping sinusoidal inputs over a range of frequencies. This series of sinusoidal signals at different frequencies can then be used to compute the frequency response. While ALICE-SA does include a sweep generator function, a sweep with many frequency points using large FFT sample sizes can take many seconds or even minutes to up-date the plot. However, FFT analysis can be used to obtain the transfer function for a network from its impulse response. We can generate a test signal with a wide frequency content, a very narrow square pulse, which will produce a plot from a single sample record at a much higher up-date rate. | ||
+ | |||
+ | **Using the FFT to get a transfer function of a system is not overly complex.** | ||
+ | |||
+ | There must be an input to the network which you can observe and record. There must be an output from the network which you can observe and record. The input and output data has to be able to be read into an analysis program, such as ALICE-SA, that can take the Fast Fourier Transform of both input and output data records. A basic concept of linear analysis is that the unit impulse response of a network and the transfer function of the network are a Laplace transform pair, or said another way, the transfer function is the Laplace transform of the unit impulse response. The implication is that we can obtain the transfer function by getting the Laplace transform of the unit impulse response. | ||
+ | |||
+ | **Practical implementation.** | ||
+ | |||
+ | If we set the number of FFT samples to 8192 the total sample time will be 81.92 mSec which is the same as one cycle at 12.2 Hz. By setting the Channel B function generator to a 12.2 Hz square wave with a very narrow duty cycle of only 4 – 6 samples wide the resulting test signal will contain frequency content every 12.2 Hz with nearly equal amplitude out to high frequencies. At 12 Hz each 10 uSec sample period is equal to about 0.012 % of duty cycle. We can set the duty cycle to anything from 0.012% to 0.08% and get similar results. The only difference is how fast the signal level falls off with increasing frequency. For a given pulse amplitude, the narrower the pulse the less energy in each 12.2 Hz spaced frequency but the flatter vs frequency they will be. The wider the pulse the more signal energy but a faster frequency roll off. 0.08% gives an acceptable frequency roll off out to 10 KHz. | ||
+ | |||
+ | The detailed settings for Channel B are as follows:\\ | ||
+ | Shape - Square\\ | ||
+ | Mode - SVMI\\ | ||
+ | VMIN = 1.3\\ | ||
+ | VMAX = 3.7 ( pulse amplitude set to allow some headroom for overshoot and ringing )\\ | ||
+ | Freq = 12.2\\ | ||
+ | Phase = 180 ( phase is set to 180 degrees to center the pulse in the time sample record )\\ | ||
+ | DutyCycle = 0.08 ( can be adjusted down to 0.012% for flatter input signal energy ) | ||
+ | |||
+ | Channel A is set in Hi-Z mode as an input. | ||
+ | |||
+ | Other Settings:\\ | ||
+ | FFT Window – Flat top ( has a wide FFT bandwidth which is wider than 12 Hz )\\ | ||
+ | FFT Samples = 8192\\ | ||
+ | Start Freq = 100 ( set to something other than 0, to ignore DC content )\\ | ||
+ | Stop Freq = 10000\\ | ||
+ | ZeroStuffing = 0 ( can be adjusted but generally has little effect on resultant plot ) | ||
+ | |||
+ | Below in figure E2 is a screen shot for the bandpass RLC configuration of figure E1. The orange trace for channel B is the narrow pulse forcing function response. The light and dark green traces are the output responses seen by channel A for C< | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | Similarly in figure E3 is a screen shot for the bandstop RLC configuration of figure E1. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
**For Further Reading:** | **For Further Reading:** |