Last revision Both sides next revision
university:tools:m1k:alice:oscilloscope-x-y-user-guide [25 Jun 2021 19:32]
Doug Mercer Add future Roll Mode info
university:tools:m1k:alice:oscilloscope-x-y-user-guide [25 Jun 2021 19:52]
Doug Mercer [The Top Menu Section]
Line 15: Line 15:
 ====The Top Menu Section==== ====The Top Menu Section====
  
-The menu section along the top contains various buttons and drop-down menus that control Oscilloscope Triggering, Horizontal time base, Horizontal position, how and what signals are displayed, and run acquisition looping / stop acquisition looping / exit program.+The menu section along the top, shown in figure 1T,  ​contains various buttons and drop-down menus that control Oscilloscope Triggering, Horizontal time base, Horizontal position, how and what signals are displayed, and run acquisition looping / stop acquisition looping / exit program.
  
 {{ :​university:​tools:​m1k:​alice:​top-buttons-0.png?​800 |}} {{ :​university:​tools:​m1k:​alice:​top-buttons-0.png?​800 |}}
  
-<WRAP centeralign>​Figure ​2, Top Menu Buttons</​WRAP>​+<WRAP centeralign>​Figure ​1T, Top Menu Buttons</​WRAP>​
  
 ===Triggering functions=== ===Triggering functions===
Line 57: Line 57:
 ===Trace Controls=== ===Trace Controls===
  
-The Curves drop down menu button allows the selection of which signal waveform traces will be displayed vs time. The All button selects all four curves to be displayed and the None button clears all four curves. Plot the Math-X and Math-Y formulas by clicking on those options. ALICE can automatically adjust the trace vertical position to center the CA-V and /or CB-V traces on the midpoint of the waveform each sweep by clicking on either or both of the options below the –Auto Vert Center- heading.+The Curves drop down menu button allows the selection of which signal waveform traces will be displayed vs time. The All button selects all four curves to be displayed and the None button clears all four curves. Plot the Math-X and Math-Y formulas by clicking on those options. ALICE can automatically adjust the trace vertical position to center the CA-V and /or CB-V traces on the midpoint of the waveform each sweep by clicking on either or both of the options below the –Auto Vert Center- heading. ​This is analogous to a software "​AC"​ coupling mode where the "​DC"​ level of the trace is always centered on the grid.  ​
  
 When using external Resistor Divider attenuators the frequency response of the Channel may be reduced. The software High Pass frequency compensation can be selected for either channel by clicking on the buttons below the –Input HP Comp- heading. See the section on Analog Inputs below When using external Resistor Divider attenuators the frequency response of the Channel may be reduced. The software High Pass frequency compensation can be selected for either channel by clicking on the buttons below the –Input HP Comp- heading. See the section on Analog Inputs below
university/tools/m1k/alice/oscilloscope-x-y-user-guide.txt · Last modified: 29 Jul 2021 14:59 by Doug Mercer