This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m1k:alice:oscilloscope-x-y-user-guide [14 Oct 2020 16:20] – [The Bottom Menu Section] Doug Mercer | university:tools:m1k:alice:oscilloscope-x-y-user-guide [05 Jan 2021 19:12] – add page on Lissajous Pattern Doug Mercer | ||
---|---|---|---|
Line 15: | Line 15: | ||
Many of the drop down menus on the main oscilloscope screen and the screens for the other instruments include accelerator keys, indicated by () around the accelerator keyboard character next to the menu item. Typing one of these characters while the mouse cursor is inside the graphics drawing area will invoke that menu function. For example typing 1 or 2 will toggle on and off the CA-V and CB-V traces. | Many of the drop down menus on the main oscilloscope screen and the screens for the other instruments include accelerator keys, indicated by () around the accelerator keyboard character next to the menu item. Typing one of these characters while the mouse cursor is inside the graphics drawing area will invoke that menu function. For example typing 1 or 2 will toggle on and off the CA-V and CB-V traces. | ||
- | By setting to 1 the EnableScopeOnly = 1; option in the alice_init.ini file, the Oscilloscope and AWG controls can be combined in one window as shown in figure 1S. The controls all work as they do in the default two window configuration. Blue arrows point to AWG related controls, green arrows point to Scope related controls. | + | By setting to 1 the EnableScopeOnly = 1; option in the alice_init.ini file, the Oscilloscope and AWG controls can be combined in one window as shown in figure 1S. The controls all work as they do in the default two window configuration |
{{ : | {{ : | ||
Line 428: | Line 428: | ||
There is also a check button to display the saved X-Y reference trace (see note above in Oscilloscope section on Snap-Shot option). | There is also a check button to display the saved X-Y reference trace (see note above in Oscilloscope section on Snap-Shot option). | ||
+ | |||
+ | {{ : | ||
=====Oscilloscope and X-Y Plot Examples: | =====Oscilloscope and X-Y Plot Examples: |