This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m1k:alice:desk-top-users-guide [31 Oct 2022 20:38] – [Command Line Interface:] Doug Mercer | university:tools:m1k:alice:desk-top-users-guide [26 Nov 2022 17:34] (current) – [Windows:] Doug Mercer | ||
---|---|---|---|
Line 38: | Line 38: | ||
* Version 1.3 [[https:// | * Version 1.3 [[https:// | ||
Download Windows Libsmu installer here: | Download Windows Libsmu installer here: | ||
- | * Version 1.0.2 for 64 bit systems | + | * Version 1.0.4 for 64 bit systems [[https:// |
- | * Version 1.0.2 for 32 bit to run ALICE [[https:// | + | * Version 1.0.4 for 32 bit systems |
The installer should include all required (python) packages but not the USB device drivers or low level interface library libsmu for the ADALM1000. The drivers can be installed by installing the Libsmu library and clicking on the install WinUSB driver box when prompted. | The installer should include all required (python) packages but not the USB device drivers or low level interface library libsmu for the ADALM1000. The drivers can be installed by installing the Libsmu library and clicking on the install WinUSB driver box when prompted. | ||
</ | </ | ||
- | Before connecting your ADALM1000 to your computer you need to install the WinUSB device drivers. On 64 bit computers (most common), run the libsmu-1.0.2-setup-x64.exe installer program. Click on the box to install the WinUSB device drivers. You may skip this step if the device drivers were installed by another package such as Pixelpulse2. | + | Before connecting your ADALM1000 to your computer you need to install the WinUSB device drivers. On 64 bit computers (most common), run the libsmu-1.0.4-setup-x64.exe installer program. Click on the box to install the WinUSB device drivers. |
- | Run the libsmu-1.0.2-setup-x86.exe installer program. Do not click on the box to install the WinUSB device drivers, that was already done by first step. If you do happen to have a version of Python and wish to write your own scripts to control the ADALM1000 then optionally install the appropriate Python bindings as well. | + | For 32 bit systems, run the libsmu-1.0.4-setup-x86.exe installer program. Do not click on the box to install the WinUSB device drivers, that was already done by first step. If you do happen to have a version of Python and wish to write your own scripts to control the ADALM1000 then optionally install the appropriate Python bindings as well. |
- | Run the alice-desktop-1.3-setup.exe installer program. ALICE desktop opens and saves info and data to various files in the installation directory. Because of user permission issues with some installations of Windows you may need to install the software in a directory other than the usual default “Program Files”. C:\ALM Software\ would be a good second choice or further down in the Documents folder. The installer adds desktop icons for each tool in the suite. Alternatively, | + | Run the alice-desktop-1.3-x64-setup.exe installer program. For 32 bit systems, run alice-desktop-1.3-x32-setup.exe installer program. ALICE desktop opens and saves info and data to various files in the installation directory. Because of user permission issues with some installations of Windows you may need to install the software in a directory other than the usual default “Program Files”. C:\ALM Software\ would be a good second choice or further down in the Documents folder. The installer adds desktop icons for each tool in the suite. Alternatively, |
- | Using the Widows executable is highly recommended but the ALICE Desktop can also be run from the Python 2.7/3.7 compatible source code with the following packages installed: | + | Using the Widows executable is highly recommended but the ALICE Desktop can also be run from the Python 2.X/3.X compatible source code with the following packages installed: |
- | Python 2.7 or Python 3.7(32 bit versions are the most tested and recommended)\\ | + | **Python 2.7 or Python 3.7**\\ |
tKinter\\ | tKinter\\ | ||
numpy numerical package extension\\ | numpy numerical package extension\\ | ||
+ | matplotlib plotting package extension\\ | ||
libsmu/ | libsmu/ | ||