This document serves as a supplemental guide to the more advanced functionality of the ALICE Desktop software interface written for use with the ADALM1000 and ADALM2000 active learning kit hardware. It is assumed that the reader has more than a passing familiarity with the Python programing language.
ALICE 1.1 and 2.0 Desktop is written in Python and includes the Numpy extension for numerical analysis. Numpy is the fundamental Python package for scientific computing. It contains among other things, a powerful array object along with a large library of high-level mathematical functions to operate on these arrays. Such as histograms, the Fourier transform, polynomial curve fitting and random number capabilities. ALICE provides the user access to these functions through a number of the interfaces such as mathematical operations on captured waveforms, including digital filters, arbitrary waveform generation, FFTs and windowing functions.
There are a number of variables that the user can use to customize the appearance of the user interface. These variables are located near the top of the Python program file. Alternatively, especially for users of the Windows executable version of ALICE Desktop, a file named alice_init.ini can be created. It should be placed in the same directory with the alice-desktop-1.1.exe executable file or the directory where the program is started. The alice_init.ini file is read, if found, when ALICE Desktop starts and before any of the windows are created. If no init file is found the internal default settings are used.
ALICE has the option to check the current firmware version and report if the version currently loaded on the board is up to date:
AllowFlashFirmware = 1 # allow user to flash new firmware on = 1, off = 0
IgnoreFirmwareCheck = 0 # Check firmware on startup on = 1, off = 0
The default text font size can be set as follows:
FontSize = 8
To improve the appearance of the desktop screens across operating systems ALICE supports Themed widgets. The theme used can be selected in the alice_init.ini file by adding or changing the following line:
Style_String = 'alt'
Where string 'alt' contains name of the desired theme. In Windows 7 and up the builtin themes are: 'winnative', 'clam', 'alt', 'default', 'classic', 'vista', 'xpnative'. For Linux the following are likely options: 'clam', 'alt', 'default', 'classic'. Mac OS X may contain others like 'aqua'. The widgets are generally configured to look the best using the 'alt' style which should be common across operating systems.
How mouse focus is controlled can be either of two modes. The default is that the focus follows the mouse such that you don't need to click inside a window to switch the mouse focus. The other mode is the opposite where the mouse focus does not follow the mouse location that is the mouse focus stays tied to selected window.
Many of the aspects of the User Interface appearance can be customized by changing the following variables from their default settings (as in these examples):
BorderSize = 1 # Border Width of frames in pixels
ButtonOrder = 0 # swap order of channel control labels
# Widget relief can be RAISED, SUNKEN, GROOVE, RIDGE, and FLAT, SOLID
ButRelief = SOLID
LabRelief = FLAT
FrameRefief = FLAT # RIDGE
GUITheme = “Light” # color theme can be “Dark” “Light” “Blue” “LtBlue” “Custom”
FrameBG = “#d7d7d7” # Med gray, frame background color
ButtonText = “#000000” # black, button text color
ButtonGreen = “#88ff88” # light green (RUN, Conn, Power, etc)
ButtonRed = “#ff8888” # light red (STOP, etc)
The mouse focus modes can be st as follows:
MouseFocus = 1 # focus follows mouse around from window to window
MouseFocus = 0 # mouse focus stays tied to selected window
Many of the buttons and controls have balloon help that appears if the mouse hovers over a control for more than a few seconds. This feature can be turned on and off by the following:
ShowBallonHelp = 0 # balloon help off
ShowBallonHelp = 1 # balloon help on
To simplify the User interface controls for each virtual instrument, other than the AWG and Time display, can be optionally enabled / disabled (1=enabled, 0=disabled):
EnableXYPlotter = 1
EnablePhaseAnalizer = 1
EnableSpectrumAnalizer = 1
EnableBodePlotter = 1
EnableImpedanceAnalizer = 1
EnableOhmMeter = 1
A simplified set of trace controls in the right side menu of the Scope screen can be optionally turned on:
ShowTraceControls = 1
By setting the following switch in the alice_init.ini file ALICE will use this much simplified “Scope Only” display configuration. The switch is set to 0 by default to access the full set of ALICE instruments. The full set of AWG controls is included in the right-hand menu area. Under the Options drop down it is possible to open an access screen to enable the rest of the vitrual instrument functionality.
EnableScopeOnly = 1
To further simplify the User interface it is possible to hide the advanced waveform Shapes in the AWG controls:
AWGShowAdvanced.set(1) # > 0 Show Advanced AWG shapes in menu
How the AWG controls are arranged is set by the global AwgLayout; AwgLayout = “Horz” variable. Side by side horizontally is the default like this:
Or by setting the variable to something other than “Horz”, such as “Vert”, can be stacked vertically like this:
Normally ALICE displays the board ID serial number at the top of each graphics display area. There is an option to supply a user specified text string instead:
LabelPlotText.set(0) # 1 = use user label string
PlotLabelText = “Custom Plot Label”
There are pairs of variables for each display window that set the size of the graphics drawing area in screen pixels. The default values are sized to optimally fill a screen with 1024×600 resolution. The menu buttons surrounding the graphics area need this much space to be properly displayed on most screens so using sizes smaller than the default may result in mangled menus.
GRW = 720 # Width of the Time grid
GRH = 390 # Height of the Time grid
GRWN = 720 # Width of the spectrum grid 720 default
GRHN = 390 # Height of the spectrum grid 390 default
GRWBP = 720 # Width of the Bode Plot grid 720 default
GRHBP = 390 # Height of the Bode Plot grid 390 default
GRWXY = 420 # Width of the XY grid 420 default
GRHXY = 390 # Height of the XY grid 390 default
GRWIA = 400 # Width of the Impedance grid 400 default
GRHIA = 400 # Height of the Impedance grid 400 default
The colors that are used to draw the various parts of the screen can be modified.
Color = “#rrggbb” rr=red gg=green bb=blue, Hexadecimal values 00 - ff
COLORframes = “#000080” # 50% blue
COLORcanvas = “#000000” # 100% black used for background color
COLORgrid = “#808080” # 50% Gray used for grid lines
COLORzeroline = “#0000ff” # 100% blue used for vertical and horizontal center grid lines
COLORtrace1 = “#00ff00” # 100% green CH A voltage trace
COLORtrace2 = “#ff8000” # 100% orange CH B voltage trace
COLORtrace3 = “#00ffff” # 100% cyan CH A current trace
COLORtrace4 = “#ffff00” # 100% yellow CH B current trace
COLORtrace5 = “#ff00ff” # 100% magenta Math trace
COLORtrace6 = “#ff0000” # 100% red
COLORtrace7 = “#8080ff” # 100% purple
COLORtraceR1 = “#008000” # 50% green CH A voltage snapshot trace
COLORtraceR2 = “#804000” # 50% orange CH B voltage snapshot trace
COLORtraceR3 = “#008080” # 50% cyan CH A current snapshot trace
COLORtraceR4 = “#808000” # 50% yellow CH B current snapshot trace
COLORtraceR5 = “#800080” # 50% magenta Math snapshot trace
COLORtraceR6 = “#800000” # 50% red
COLORtraceR7 = “#4040a0” # 70% purple
COLORtext = “#ffffff” # 100% white used for Text display
COLORtrigger = “#ff0000” # 100% red used for trigger point
COLORsignalband = “#ff0000” # 100% red
COLORzeroline; COLORzeroline = “#0000ff”
Variable for selecting grid background color:
ColorMode.set(0) # = 0 black grid background, white text > 0 white grid background, black text
Sets COLORcanvas and COLORtext variables.
Variable for width of grid lines in pixels:
GridWidth = 1
Value for on board resistors and external AD584 reference used in the self calibration procedure:
OnBoardRes = 50.83
AD584act = 2.5
Default math equations, These initialize the entry spaces the first time each matching dialog pop-up window opens.
MathString = “(VBuffA[t] + VBuffB[t] - CHAOffset)“
MathXString = ”(VBuffA[t] - CHAOffset)“
MathYString = ”(VBuffB[t] - CHBOffset)“
UserAString = “MaxV1-VATop”
UserALabel = “OverShoot”
UserBString = “MinV2-VBBase”
UserBLabel = “UnderShoot”
MathAxis = “V-A” # can be one of the following “V-A”, “V-B”, I-A”, “I-B”
MathXAxis = “V-A”
MathYAxis = “V-B”
AWGAMathString = ”(VBuffA + VBuffB)/2“
AWGBMathString = ”(VBuffA + VBuffB)/2“
FFTUserWindowString = “numpy.kaiser(SMPfft, 14) * 3”
DigFilterAString = “numpy.sinc(numpy.linspace(-1, 1, 91))“
DigFilterBString = “numpy.sinc(numpy.linspace(-1, 1, 91))”
Inside the alice_init.ini any of these variables can be set using the example format shown here:
GRW = 720
GRH = 390
GRWN = 720
GRHN = 390
GRWXY = 420
GRHXY = 390
GRWIA = 400
GRHIA = 400
User entry widgets can optionally be added to the Time (scope) and X-Y screens by setting the following variable in the init file:
EnableUserEntries = 1
The two Time user entries can be accessed using User1Entry.get(), User2Entry.get() variables and the two X-Y user entries can be accessed using User3Entry.get(), User4Entry.get() variables.
The optional software interfaces can be enabled or disabled by setting the following variables to either 1 or 0 in the alice_init.ini file.
EnableDigIO = 1
EnableCommandInterface = 0
EnableMuxMode = 1
EnableMinigenMode = 0
EnablePIODACMode = 0
EnablePmodDA1Mode = 0
EnableDigPotMode = 0
EnableGenericSerialMode = 0
EnableAD5626SerialMode = 0
EnableDigitalFilter = 0
EnableMeasureScreen = 0
EnableETSScreen = 0
EnableHSsampling = 0
ALICE uses a large number of variables and arrays to hold both the captured data as well as the results of calculations performed on the data. Below is a list of the variable and array names with explanations of their use and how they are calculated. Endsample = Last sample in Buffer
hldn = number of samples from start of buffer to ignore based on Hold Off time setting.
Waveform calculated Vertical measurement constants:
Channel A Average voltage, DCV1 = numpy.mean(VBuffA[hldn:Endsample])
Channel A Minimum voltage, MinV1 = numpy.amin(VBuffA[hldn:Endsample])
Channel A Maximum voltage, MaxV1 = numpy.amax(VBuffA[hldn:Endsample])
Channel A Top voltage, VATop is the voltage of the most positive peak in the histogram
Channel A Base voltage, VABase is the voltage of the least positive peak in the histogram
Channel A RMS voltage, SV1 = numpy.sqrt(numpy.mean(numpy.square(VBuffA[hldn:Endsample])))
Channel B Average voltage, DCV2 = numpy.mean(VBuffB[hldn:Endsample])
Channel B Minimum voltage, MinV2 = numpy.amin(VBuffB[hldn:Endsample])
Channel B Maximum voltage, MaxV2 = numpy.amax(VBuffB[hldn:Endsample])
Channel B Top voltage, VBTop is the voltage of the most positive peak in the histogram
Channel B Base voltage, VBBase is the voltage of the least positive peak in the histogram
Channel B RMS voltage, SV2 = numpy.sqrt(numpy.mean(numpy.square(VBuffB[hldn:Endsample])))
Channel A Average current in mA, DCI1 = numpy.mean(IBuffA[hldn:Endsample])*1000
Channel A Minimum current in mA, MinI1 = numpy.amin(IBuffA[hldn:Endsample]) ])*1000
Channel A Maximum current in mA, MaxI1 = numpy.amax(IBuffA[hldn:Endsample]) ])*1000
Channel A RMS current in mA, SI1 = numpy.sqrt(numpy.mean(numpy.square(IBuffA[hldn:Endsample])))*1000
Channel B Average current in mA, DCI2 = numpy.mean(IBuffB[hldn:Endsample])*1000
Channel B Minimum current in mA, MinI2 = numpy.amin(IBuffB[hldn:Endsample])
Channel B Maximum current in mA, MaxI2 = numpy.amax(IBuffB[hldn:Endsample])
Channel B RMS current in mA, SI2 = numpy.sqrt(numpy.mean(numpy.square(IBuffB[hldn:Endsample])))*1000
Waveform calculated Horizontal measurement constants:
CHAHW is the channel A High Pulse Width
CHALW is the channel A Low Pulse Width
CHADCy is the channel A Duty Cycle
CHAperiod is the channel A Period
CHAfreq is the channel A Frequency
CHABphase is the channel A to channel B relative phase angle
CHBHW is the channel B High Pulse Width
CHBLW is the channel B Low Pulse Width
CHBDCy is the channel B Duty Cycle
CHBperiod is the channel B Period
CHBfreq is the channel B Frequency
Captured Data Waveform Buffers:
VBuffA is the Channel A voltage sample array ( in volts )
VBuffB is the Channel B voltage sample array ( in volts )
IBuffA is the Channel A current sample array ( in amps, multiply by 1000 for mA )
IBuffB is the Channel B current sample array ( in amps, multiply by 1000 for mA )
VmemoryA is the Channel A voltage memory array used for Trace Averaging
VmemoryB is the Channel B voltage memory array used for Trace Averaging
ImemoryA is the Channel A current memory array used for Trace Averaging
ImemoryB is the Channel B current memory array used for Trace Averaging
HBuffA contains the histogram of the channel A voltage waveform
HBuffB contains the histogram of the channel B voltage waveform
VBuffMA is the Mux Mode A channel voltage sample array ( in volts )
VBuffMB is the Mux Mode B channel voltage sample array ( in volts )
VBuffMC is the Mux Mode C channel voltage sample array ( in volts )
VBuffMD is the Mux Mode D channel voltage sample array ( in volts )
t is the time index ( 10 uSec per point )
SAMPLErate is the sampling rate, 100000 samples per Sec, or 10 uSec per sample
Vertical Position variables:
CHAOffset is the value in the channel A voltage position entry window
CHBOffset is the value in the channel B voltage position entry window
CHAIOffset is the value in the channel A current position entry window
CHBIOffset is the value in the channel B current position entry window
AWG waveform arrays:
AWGAwaveform is the Channel A AWG waveform memory array (used for non-built in waveforms)
AWGBwaveform is the Channel B AWG waveform memory array (used for non-built in waveforms)
The following example Python syntax allows setting the start and stop points to be used in an array:
AWGAwaveform[ start : stop ] where start and stop are integers.
Digital Filter coefficients:
DFiltACoef # Scope channel A Digital filter coefficients
DFiltBCoef # Scope channel B Digital filter coefficients
AWGFiltACoef # AWG channel A Digital filter coefficients
AWGFiltBCoef # AWG channel B Digital filter coefficients
Use Example: VBuffA = numpy.convolve(VBuffA, DFiltACoef)
Frequency domain buffers:
FFTresultA contains the Channel A voltage magnitude FFT frequency bin results. To get the results in dB the following formula is used:
dbA = (10 * math.log10(float(FFTresultA[n])) + 17) # gives amplitude in dBVolts where 0 dB = 1 Vrms
FFTresultB, Same for Channel B
FFTmemoryA is the Channel A FFT memory array used for Trace Averaging and Peak Hold modes
FFTmemoryB, Same for Channel B
SMPfft is the number of samples used when the FFT is calculated. It will always be a power of 2. And it will be the length of the FFT window function array.
Bode Plotter arrays:
FSweepAdB contains the Channel A voltage magnitude Bode plot frequency sweep results. To get the results in dB the following formula is used:
dbA = (10 * math.log10(float(FSweepAdB[n])) + 17)
FSweepBdB, Same for Channel B
FSweepAPh, Channel A Phase in degrees
FSweepBPh, Same for Channel B
One of the AWG waveforms that can be constructed is the Fourier series of cosines for a square wave.
The routine starts by first making the cosine wave at the fundamental frequency:
AWGAwaveform = numpy.cos(numpy.linspace(0, 2*numpy.pi, SAMPLErate/AWGAFreqvalue))
It then loops over k ( only odd numbers ), the number of requested terms, calculating the harmonic and adding it to the waveform:
Harmonic = (math.sin(k*numpy.pi/2)/k)*(numpy.cos(numpy.linspace(0, k*2*numpy.pi, SAMPLErate/AWGAFreqvalue)))
AWGAwaveform = AWGAwaveform + Harmonic
After all the harmonic terms have been added the waveform is scaled and offset based on the entered Min and Max values.
# def AWGAMakeFourier(): global AWGAwaveform, AWGSAMPLErate, AWGAAmplvalue, AWGAOffsetvalue, AWGALength global AWGADutyCyclevalue, AWGAFreqvalue, duty1lab, AWG_Amp_Mode # 0 = Min/Max mode, 1 = Amp/Offset global AWGA2X, AWG_2X, SAMPLErate, BaseSampleRate global AWGA_Ext_Gain, AWGA_Ext_Offset, AWGB_Ext_Gain, AWGB_Ext_Offset BAWGAAmpl(0) BAWGAOffset(0) BAWGAFreq(0) BAWGADutyCycle(0) Max_term = int(AWGADutyCyclevalue*100) if AWG_2X.get() == 1: TempRate = (BaseSampleRate*2) else: TempRate = BaseSampleRate AWGAwaveform = [] AWGAwaveform = numpy.cos(numpy.linspace(0, 2*numpy.pi, int(TempRate/AWGAFreqvalue))) # the fundamental k = 3 while k <= Max_term: # Add odd harmonics up to max_term Harmonic = (math.sin(k*numpy.pi/2.0)/k)*(numpy.cos(numpy.linspace(0, k*2*numpy.pi, int(TempRate/AWGAFreqvalue)))) AWGAwaveform = AWGAwaveform + Harmonic k = k + 2 # skip even numbers if AWG_Amp_Mode.get() == 0: amplitude = (AWGAOffsetvalue-AWGAAmplvalue)/2.0 offset = (AWGAOffsetvalue+AWGAAmplvalue)/2.0 else: amplitude = AWGAAmplvalue*AWGA_Ext_Gain.get() offset = (AWGAOffsetvalue * AWGA_Ext_Gain.get()) + AWGA_Ext_Offset.get() AWGAwaveform = (AWGAwaveform * amplitude) + offset # scale and offset the waveform SplitAWGAwaveform() duty1lab.config(text="Harmonics") BAWGAPhaseDelay() UpdateAwgCont() #
ALICE includes the numpy built in functions to save and load the contents of any array to a file using the Command Line interface or inside a script file. These are in addition to the ( behind the scenes ) ways provided under the File drop down and other menus.
To use the numpy function to save an array ( the VBUffA channel A voltage waveform buffer for example ) to a .csv file you would type in the Command Line interface:
numpy.savetxt('scope_data.csv', VBuffA, delimiter=',', fmt='%2.4f')
Where “scope_data.csv” is the name of the destination file, VBuffA is of course the data array to save, delimiter=”,” tells the function to use a , to separate the columns ( there won’t be multiple columns since most ALICE arrays are one dimensional ) and fmt=‘%2.4f’ sets the format to 4 decimal places.
To use the numpy function to load an array ( the AWGAwaveform AWG A waveform buffer for example ) from a .csv file you would type in the Command Line interface:
numpy.loadtxt('awg_data.csv')
A second way to save data is a wrapper function around the Python wave package. For example, to save the VBuffA array ( channel A voltage waveform buffer ) to a mono .wav file ( at 100 KSPS ) you would type in the Command Line interface:
Write_WAV(VBuffA, 2, “my_data.wav”)
Where “my_data.wav” is the name of the destination file, VBuffA is of course the data array to save, and the 2 tells the program to save two copies of the array data to the file for example. This is handy to make longer versions of the relatively short buffer lengths, used in ALICE, that can be listened to by playing back the .wav file.
ALICE contains a number of special functions that can be used to measure, generate and manipulate waveform array data samples.
Multi-sine signals are often used in frequency response measurements of a network or system,
Schroeder Multi-sine:
In 1970, Schroeder published a method for reducing the crest factor of multi-sine signals with flat amplitude spectra and equally spaced frequency components by choosing the phases φk such that φk=−k(k−1)π/k. The typical crest factor of a Schroeder multi-sine with flat amplitude spectra and uniformly spaced frequency components is approximately 1.6.
The function returns an array of sample points of length Length, scaled by Ampl. The lowest, first tone has a period of Length samples. NrTomes integer multiples of the first tomes are generated.
def SchroederPhase(Length, NrTones, Ampl): # Generate a Schroeder Phase (Chirp) of Length samples and having NrTones OutArray = [] OutArray = Ampl*numpy.cos(numpy.linspace(0, 2*numpy.pi, Length)) # the fundamental k = 2 while k <= NrTones: # Add all harmonics up to NrTones Harmonic = Ampl*numpy.cos(numpy.linspace(0, k*2*numpy.pi, Length)+(numpy.pi*k*k/NrTones)) OutArray = OutArray + Harmonic k = k + 1 OutArray = OutArray + 2.5 # Center wavefrom on 2.5 V return(OutArray) #
Generating Test Noise waveforms
Time-series From Half-spectrum:
It is often useful to be able to produce not only flat, but arbitrary noise spectrum profiles - flat “bands” of noise, “pink noise”, “noise mountains” emulating peaking in some amplifiers. The Generate Time-series From Half-spectrum code block starts with a desired noise spectral density (which can be generated manually or from simulation), the sample rate of the time series, and produces a time series of voltage values that can be then played back through the AWG.
# # Generate Time-series From Half-spectrum code block # takes: a desired noise spectral density array (freq) # the sample rate of the time series (fs), # returns a time series of voltage samples that can be sent to the AWG # # DC in first element. # Output length is 2x input length def time_points_from_freq(freq, fs=1, density=False): N=len(freq) rnd_ph_pos = (numpy.ones(N-1, dtype=numpy.complex)* numpy.exp(1j*numpy.random.uniform (0.0,2.0*numpy.pi, N-1))) rnd_ph_neg = numpy.flip(numpy.conjugate(rnd_ph_pos)) rnd_ph_full = numpy.concatenate(([1],rnd_ph_pos,[1], rnd_ph_neg)) r_s_full = numpy.concatenate((freq, numpy.roll(numpy.flip(freq), 1))) r_spectrum_rnd_ph = r_s_full * rnd_ph_full r_time_full = numpy.fft.ifft(r_spectrum_rnd_ph) # print("RMS imaginary component: ", # np.std(np.imag(r_time_full)), # " Should be close to nothing") if (density == True): #Note that this N is "predivided" by 2 r_time_full *= N*numpy.sqrt(fs/(N)) return(numpy.real(r_time_full))
Some examples that use time_points_from_freq
# def TimeSeriesNoise(n, Fsample, mag, b=4): # Build Noise Time-series # n = number of Freq Bins # b = number of noise bands # Fsample is Sample Rate # generates four "bands" of mag V/rootHz noise mag = mag * 0.707106 # scale by 1/sqrt 2 for RMS width = int(n/(4 * b)) i = 1 aband = numpy.ones(width) zband = numpy.zeros(width) bands = numpy.concatenate((aband, zband)) while i < b: bands = numpy.concatenate((bands, aband, zband)) i = i + 1 bands = bands*mag bands[0] = 0.0 # Set DC bin content to zero return time_points_from_freq(bands, fs=Fsample, density=True) #
# # Generate Time samples for single frequency Bin # Uses IFFT # def TimeSeriesSingleTone(n, BinNum, Fsample, mag): # Build Single tone Time-series # n = number of Freq Bins # BinNum = FFT Bin number # Fsample is Sample Rate # mag is tone amplitude bands = numpy.zeros(n) bands[BinNum] = 1 bands = bands * (mag/2.0) return time_points_from_freq(bands, fs=Fsample, density=True)
Colored Noise Generators
def PinkNoise(N, mag): # Pink noise. # Pink noise has equal power in bands that are proportionally wide. # Power spectral density decreases with 3 dB per octave. # N Length of sample array, mag magnitude scaling factor x = numpy.random.normal(0.0, 1, N).astype(numpy.float32) # white Noise X = numpy.fft.rfft(x) / N S = numpy.sqrt(numpy.arange(X.size)+1.0) # +1 to avoid divide by zero y = numpy.fft.irfft(X/S).real[:N] # extremely tiny value 1e-9 without normalization z = numpy.ndarray = mag y = y * numpy.sqrt((numpy.abs(z)**2).mean() / (numpy.abs(y)**2).mean()) return y
def BlueNoise(N, mag): # Blue noise. # Power increases with 6 dB per octave. # Power spectral density increases with 3 dB per octave. # N Length of sample array, mag magnitude scaling factor x = numpy.random.normal(0.0, 1, N).astype(numpy.float32) # white Noise X = numpy.fft.rfft(x) / N S = numpy.sqrt(numpy.arange(X.size)) # Filter y = numpy.fft.irfft(X*S).real[:N] z = numpy.ndarray = mag y = y * numpy.sqrt((numpy.abs(z)**2).mean() / (numpy.abs(y)**2).mean()) return y
def BrownNoise(N, mag): # Brown noise. # Power decreases with -3 dB per octave. # Power spectral density decreases with 6 dB per octave. # N Length of sample array, mag magnitude scaling factor x = numpy.random.normal(0.0, 1, N).astype(numpy.float32) # white Noise X = numpy.fft.rfft(x) / N S = numpy.arange(X.size)+1 # Filter y = numpy.fft.irfft(X/S).real[:N] z = numpy.ndarray = mag y = y * numpy.sqrt((numpy.abs(z)**2).mean() / (numpy.abs(y)**2).mean()) return y
def VioletNoise(N, mag): # Violet noise. # Power increases with +9 dB per octave. # Power density increases with +6 dB per octave. # N Length of sample array, mag magnitude scaling factor x = numpy.random.normal(0.0, 1, N).astype(numpy.float32) # white Noise X = numpy.fft.rfft(x) / N S = numpy.arange(X.size) # Filter y = numpy.fft.irfft(X*S).real[0:N] z = numpy.ndarray = mag y = y * numpy.sqrt((numpy.abs(z)**2).mean() / (numpy.abs(y)**2).mean()) return y
Digital single pole RC filter
This function is used mainly for compensating the response of any analog input resistor divider networks placed ahead of the analog inputs but can be used for any other filtering needs such as filtering AWG waveforms. The “RC” time constant is passed in uSec and the Gain can be either positive for high pass function or negative for low pass function.
## Digital RC filter function for input divider frequency compensation # TC1 is in micro seconds def Digital_RC_High_Pass( InBuff, TC1, Gain ): global SAMPLErate, Two_X_Sample OutBuff = [] n = len(InBuff) if Two_X_Sample.get() == 0: Delta = 1.0/SAMPLErate else: # adjust for sligh difference in 2X sample mode? Delta = 0.88/SAMPLErate TC = TC1 * 1.0E-6 Alpha = TC / (TC + Delta) OutBuff.append(0.0) # initialize first output sample i = 1 while i < n: OutBuff.append( Alpha * (OutBuff[i-1] + InBuff[i] - InBuff[i-1]) ) i += 1 OutBuff = numpy.array(OutBuff) OutBuff = InBuff + (OutBuff * Gain) return OutBuff
Digital Filter Coefficient Generators
Higher order SINC filters can be generated by convolving SINC1 filters. For example, convolving two SINC1 filters (with a rectangular impulse response in time) will result in a SINC2 response, with a triangular impulse response.
# # Higher order SINC filters can be generated by convolving first order Box Car filters def BuildRejectFilter(Order, Freject, Fsample): # Order can be 1, 2, 3 or 4 # Fsample = 100000 # Calculate SINC1 oversample ratios for Freject osr = int(Fsample/Freject) # # osr60 = int(Fsample/60) # 60 Hz example # Create "boxcar" SINC1 filter sinc1 = numpy.ones(osr) # sinc1_60 = np.ones(osr60) # Calculate higher order filters sinc2 = numpy.convolve(sinc1, sinc1) sinc3 = numpy.convolve(sinc2, sinc1) sinc4 = numpy.convolve(sinc2, sinc2) fosr = float(Fsample/Freject) if Order == 1: return sinc1/fosr elif Order == 2: return sinc2/fosr elif Order == 3: return sinc3/fosr elif Order == 4: return sinc4/fosr else: return sinc1/fosr # Here's the SINC4-ish filter # with three zeros at 50Hz, one at 60Hz. # filt_50_60_rej = np.convolve(sinc3_50, sinc1_60)
Rearranging the order of samples:
Sometimes there is a need to rearrange the data samples in an array. The length of the array is not changed just the order of the samples. These two functions, Wrap and Unwrap, are inverses of each other.
def Wrap(InArray, WrFactor): # Build new array by skipping WrFactor samples and wrapping back around # [1,2,3,4,5,6} becomes [1,3,5,2,4,6] # effectively multiplies the frequency content by WrFactor OutArray = [] OutArray = numpy.array(OutArray) InArray = numpy.array(InArray) EndIndex = len(InArray) StartIndex = 0 while StartIndex < WrFactor: OutArray = numpy.concatenate((OutArray, InArray[StartIndex:EndIndex:WrFactor]), axis=0) StartIndex = StartIndex + 1 return OutArray #
def UnWrap(InArray, WrFactor): # Build new array by splitting arrray into WrFactor sections and interleaving samples from each section # [1,2,3,4,5,6} becomes [1,4,2,5,3,6] # effectively divided the frequency content by WrFactor OutArray = [] InArray = numpy.array(InArray) EndIndex = int(len(InArray)/WrFactor) StartIndex = 0 while StartIndex < EndIndex: LoopIndex = 0 while LoopIndex < WrFactor: OutArray.append(InArray[StartIndex+LoopIndex]) LoopIndex = LoopIndex + 1 StartIndex = StartIndex + 1 OutArray = numpy.array(OutArray) return OutArray #
The following function opens a .wav audio file and writes the passed array of samples to it.
def Write_WAV(data, repeat, filename): global SAMPLErate # write data array to mono .wav file 100KSPS # copy buffer repeat times in output file # Use : Write_WAV(VBuffB, 2, "write_wave_1.wav") wavfile = wave.open(filename, "w") nchannels = 1 sampwidth = 2 framerate = SAMPLErate amplitude = 32766 nframes = len(data) comptype = "NONE" compname = "not compressed" wavfile.setparams((nchannels, sampwidth, framerate, nframes, comptype, compname)) # Normalize data ArrN = numpy.array(data) ArrN /= numpy.max(numpy.abs(data)) frames = [] for s in ArrN: mul = int(s * amplitude) # print "s: %f mul: %d" % (s, mul) frames.append(struct.pack('h', mul)) print( len(frames)) frames = ''.join(frames) print( len(frames)) for x in xrange(0, repeat): print( x ) wavfile.writeframes(frames) wavfile.close() #
Calculation Relative Phase
There are a number of possible ways to measure the phase difference between two signals. The main method used by the ALICE measurements is by finding “zero-crossing” points in each waveform and calculating the phase from the time samples. A second method, used in the Phase Analyzer tool ( and Bode plotter) is the FFT. The following function calculates the relative based on this formula:
However, the results are incorrect if either of the two signals has a DC offset. The function removes any DC content. Also the result is only from 0 to +180º. It lacks quadrature calculation for a definitive + or - sign for the phase, which requires a bit more calculation.
This method is strictly speaking only for use with sine wave signals of the same frequency but results for triangle waves is reasonably close and for square waves is only correct at 0 and 180º.
# Function to calculate relative phase angle between two sine waves of the same frequency # Removes any DC content def Sine_Phase(): global DCV1, DCV2, VBuffA, VBuffB sum1 = 0.0 sum2 = 0.0 sum12 = 0.0 i = 0 n = len(VBuffA) while i < n: sum1 += (VBuffA[i]-DCV1)*(VBuffA[i]-DCV1) sum2 += (VBuffB[i]-DCV2)*(VBuffB[i]-DCV2) sum12 += (VBuffA[i]-DCV1)*(VBuffB[i]-DCV2) i += 1 return math.acos(sum12/math.sqrt(sum1*sum2))*180.0/numpy.pi #
Curve Fitting
The numpy library contains a polynomial fitting function. The following exponential curve fitting function is contained in ALICE.
# Fit the function y = A * exp(B * x) to the data arrays xs and ys # returns (A, B) # From: https://mathworld.wolfram.com/LeastSquaresFittingExponential.html def fit_exp(xs, ys): S_x2_y = 0.0 S_y_lny = 0.0 S_x_y = 0.0 S_x_y_lny = 0.0 S_y = 0.0 for (x,y) in zip(xs, ys): S_x2_y += x * x * y S_y_lny += y * numpy.log(y) S_x_y += x * y S_x_y_lny += x * y * numpy.log(y) S_y += y #end a = (S_x2_y * S_y_lny - S_x_y * S_x_y_lny) / (S_y * S_x2_y - S_x_y * S_x_y) b = (S_y * S_x_y_lny - S_x_y * S_y_lny) / (S_y * S_x2_y - S_x_y * S_x_y) return (numpy.exp(a), b) #
As an example use case the following simple resistor and diode circuit shown in figure 1 is offered.
Figure 1, Diode test circuit
The voltage across a small signal diode is measured using scope channel B and the diode current is measured using the AWG A channel current as the channel A voltage is swept using a triangle wave. The data samples in the VBuffB and IBuffA arrays is used to fit an exponential. In the following ALICE script, the data is analyzed and then plotted using the built-in pyplot functions from the Matplotlib library.
Alternatively these lines can be commented out and the values simply printed to the Console screen.
xs = VBuffB[50:500] # diode voltage ys = IBuffA[50:500] # diode current ys = ys / 1000.0 # convert mA to Amps ys = numpy.absolute(ys) # make all y values positive for taking ln ys = ys - numpy.amin(ys) + 2.2e-9 # add offset and Is guess # Function to fit data I_d(x) + I_s = I_s * exp(x/(n*Vt)) # note that I_d + I_s is approx I_d since I_s is small (A, B) = fit_exp(xs, ys) # some constants # Saturation current I_s = 1.0e-9 # Ideality factor n = 2 # Thermal voltage, KT/q Vt = 0.0259 # guess values for Is and n # Iguess(x) = 5.0e-9*(exp(x/(2*Vt))-1.0) #print( "{Is} A = ", A, "B = ", B ) Fit_N = 1.0/(Vt*B) # Fit n with Vt at 25 C Is_String = ' {0:.2e} '.format(A) AmA = A * 1000.0 User3Entry.delete(0,END) User3Entry.insert(5, Is_String) N_String = ' {0:.2f} '.format(Fit_N) User4Entry.delete(0,END) User4Entry.insert(5, N_String) #print ("Vt = ", Vt, "Fit Vt = ", Fit_Vt) plt.figure() plt.plot(VBuffB[0:500], IBuffA[0:500], 'g', label='Raw Data') plt.plot(VBuffB[0:500], [AmA * (numpy.exp(B*x)-1) for x in VBuffB[0:500]], 'b', label='Fit') #plt.plot(xs, [2.2e-9 * (numpy.exp(x/(2.0*0.0259))-1) for x in xs], 'r', label='Guess') plt.title('Exponential Diode Fit') plt.xlabel('Volts') plt.ylabel('Amps') plt.legend(loc='best') plt.tight_layout() plt.show(block=False)
The following screenshots show the results:
Figure 2, Time waveforms
Figure 3, V-I X,Y plot
Figure 4, Curve fit results
ALICE includes the Numpy numerical library of array creation and manipulation functions. The reader is directed to the numpy documentation for complete details on these functions. Here we will point out some of the more useful functions for creating and manipulating waveform sample arrays. Numpy contains many more than can be covered here. However, be sure to only use functions that return 1 dimensional arrays.
In these example we use AWGAwaveform as the array variable but any of the ALICE internal waveform arrays can be of course used.
numpy.ones(length) Return a new array of given length filled with ones.
numpy.zeros(length) Return a new array of given length filled with zeros.
numpy.full(length, fill_value) Return a new array of given length, filled with fill_value.
numpy.linspace(start_value, stop_value, num=length) Return a new array of given length of evenly spaced numbers between start_value and stop_value.
numpy.logspace(start_value, stop_value, num=length, base=log_base) Return a new array of given length of numbers spaced evenly on a log scale. The base of the log can be optionally specified such as 10 or 2 etc.
numpy.square(x) Return the element-wise square of the input.
numpy.sqrt(x) Return the positive square-root of an array, element-wise.
numpy.exp(x) Calculate the exponential of all elements in the input array.
numpy.log(x) Return the Natural logarithm, element-wise.
numpy.log10(x) Return the base 10 logarithm of the input array, element-wise.
numpy.sin(x) Trigonometric Sine, element-wise.
numpy.cos(x) Cosine element-wise.
To create one cycle of a sine wave 400 samples long you will first create an array of values from 0 to 2*pi and then send it to the sine function like this.
numpy.sin(numpy.linspace(0, 2*numpy.pi, 400))
The waveform values will be from -1 to 1 so additionally you will need to scale and or offset the values to be between 0 than 5 for the AWG. In this example we create the sine wave centered on 2.5 V with a P-P of 4 V.
(numpy.sin(numpy.linspace(0, 2*numpy.pi, 400)) * 2) + 2.5
numpy.sinc(x) Return the sinc function.
Much like the trig functions the input to the sinc function is a linear spaced array of points.
numpy.sinc(numpy.linspace(-4, 4, 400)) will product 4 “cycles” 400 samples long.
The values will be between -1 to 1 so additionally you will need to scale and or offset the values to be between 0 than 5 for the AWG. In this example we create the sinc pulse centered on 2.5 V with a peak value of 4.5 V.
(numpy.sinc(numpy.linspace(-4, 4, 400)) * 2)+2.5
Many of the random number functions return arrays of random numbers. Here are a few examples:
numpy.random.standard_normal(8000)+2.5 will return a 8,000 sample array of random numbers with a normal distribution, standard deviation = 1, centered on 2.5.
numpy.random.uniform(1,4,10000) will return a 10,000 sample array of random numbers with a uniform distribution between 1 and 4.
numpy.random.triangular(1, 2.5, 4, 10000) will return a 10,000 sample array of random numbers with a triangular distribution between 1 and 4, centered on 2.5.
numpy.roll(AWGAwaveform, shift) Roll array elements by shift points. This will in effect change the relative timing delay or phase of the waveform.
numpy.flip(AWGAwaveform) Reverse the order of elements in an array. This will reverse the order of the time samples in the array.
numpy.concatenate( (AWGAwaveform, AWGBwaveform, … ) ) Join a sequence of arrays.
numpy.repeat(AWGAwaveform, repeats) Repeat elements of an array. This will effectively lower the sample rate of the waveform. If repeat is 2 the frequency of the new waveform will be ½ what the original was.
The pad function adds samples to the beginning and end of the array.
numpy.pad(AWGAwaveform, (100, 100), ‘edge’)
numpy.pad(AWGAwaveform, (100,100), ‘maximum’)
The first argument is the array variable, next is a list of the number of points to add. In the case of our one dimensional waveforms this is just two values for the beginning and end of the array. The third argument tells the function what values to use to extend the array. How the array is extended can be one of the following:
‘constant’ - Pads with a constant value.
‘edge’ - Pads with the edge values of array.
‘linear_ramp’ - Pads with the linear ramp between end_value and the array edge value.
‘maximum’ - Pads with the maximum value of all or part of the vector along each axis.
‘mean’ - Pads with the mean value of all or part of the vector along the axis.
‘median’ - Pads with the median value of all or part of the vector along the axis.
‘minimum’ - Pads with the minimum value of all or part of the vector along the axis.
‘reflect’ - Pads with the reflection of the vector mirrored on the first and last values of the vector along the axis.
‘symmetric’ - Pads with the reflection of the vector mirrored along the edge of the array.
‘wrap’ - Pads with the wrap of the vector along the axis. The first values are used to pad the end and the end values are used to pad the beginning.
numpy.bartlett(length) Return the Bartlett window.
numpy.blackman(length) Return the Blackman window.
numpy.hamming(length) Return the Hamming window.
numpy.hanning(length) Return the Hanning window.
numpy.kaiser(length, beta) Return the Kaiser window
numpy.convolve(a, v) Returns the discrete, linear convolution of two one-dimensional sequences.
This is used primarily for digital filtering of waveform data arrays.
numpy.polyfit(x, y, deg) Fit a polynomial p(x) = p[0] * x^deg + … + p[deg] of degree deg to points (x, y). Returns a vector of coefficients p that minimizes the squared error.
numpy.poly1d(p) A convenience class, used to encapsulate “natural” operations on polynomials so that said operations may take on their customary form in code.
The following example shows how to use polyfit and poly1d to fit a 5th order polynomial to the voltage characteristics of diode and plot the polynomial over the plot of the measured data points.
First construct the simple resistor and diode circuit shown in the figure.
Figure, Diode test circuit
Set Channel A AWG Min value to 0V and Max value to 5V. Set the Mode to SVMI and the Shape to triangle. Set the Freq to 100 Hz. Set Channel B mode to Hi-Z to measure the voltage across the diode.
Set the Horz Time scale to 0.5mSec/Div. Hit Run, wait for a few seconds to capture some data then hit Stop. This should display the rising half of the triangle wave on Channel A from 0 to 5 V ( green trace ). The width of the grid will be 500 sample points ( 5 mSec at 10 uSec/sample). Channel B should display the voltage across the diode going from 0 to about 0.8 V ( orange trace ). You may want to change the vertical scale to 0.1 V/div and position to 0.5 for CH-B to display the waveform from 0 to 1 V. You should now have something like this:
Plot of Diode Voltage
Open the Command Line interface ( with the program stopped ). We want to fit a polynomial to the first 500 samples where CH-A ramps from 0 to 5 V. Type the following line into the entry space and hit return.
global Zpoly; Zpoly = numpy.polyfit(VBuffA[0:499], VBuffB[0:499], 5)
To check the terms of the polynomial type the following line into the entry space and hit return.
print Zpoly
In the ALICE desktop console window you should see something like this.
ALICE console showing polynomial terms
We can use poly1d to make an object that makes this easy to plot on the screen. Type the following line into the entry space and hit return.
global ZBuff; ZBuff = numpy.poly1d(Zpoly)
Again to check the results type the following line into the entry space and hit return.
print ZBuff
In the ALICE desktop console window you should now see something like this.
ALICE console showing polynomial equation
To plot the polynomial on the screen we will use the Math waveform feature. From the Math drop down menu select Math Axis and set it to V-B to use the same axis as the diode voltage plot. From the Math drop down menu select Enter Formula and enter the following:
ZBuff(VBuffA[t])-CHBOffset
This plots the value of the polynomial evaluated at each point in VBuffA as the time index t goes from 0 to 499 ( 5 mSec ). Be sure to note that () are used for ZBuff and not [] because it is a function and not an array like VBuffA. You should now see something like this on the display. The magenta Math plot is the polynomial.
Plot of measured data and polynomial
For completeness, here are a few of the more obscure arrays used in ALICE:
These trace “lines” are 2d X-Y arrays in screen pixels.
T1Vline = [] # Voltage Trace line channel A
T2Vline = [] # Voltage Trace line channel B
T1Iline = [] # Current Trace line channel A
T2Iline = [] # Current Trace line channel B
TMAVline = [] # Voltage Trace line MUX channel A
TMBVline = [] # Voltage Trace line MUX channel B
TMCVline = [] # Voltage Trace line MUX channel C
TMDVline = [] # Voltage Trace line MUX channel D
TMBRline = [] # V reference Trace line MUX channel B
TMCRline = [] # V reference line MUX channel C
TXYline = [] # XY Trace line
TXYRline = [] # XY reference trace line
Tmathline = [] # Math trace line
T1VRline = [] # V reference Trace line channel A
T2VRline = [] # V reference Trace line channel B
T1IRline = [] # I reference Trace line channel A
T2IRline = [] # I reference Trace line channel B
TMRline = [] # Math reference Trace line
T1Fline = [] # Frequency Trace line channel A
T2Fline = [] # Frequency Trace line channel B
T1Pline = [] # Phase angle Trace line channel A - B
T2Pline = [] # Phase angle Trace line channel B - A
T1FRline = [] # F reference Trace line channel A
T2FRline = [] # F reference Trace line channel B
T1PRline = [] # Phase reference Trace line channel A - B
T2PRline = [] # Phase reference Trace line channel B - A
TFMline = [] # Frequency Math Trace
TFRMline = [] # Frequency reference Math Trace
TAFline = [] # Bode Freq Trace line channel A
TBFline = [] # Bode Freq Trace line channel B
TAPline = [] # Bode Phase angle Trace line channel A - B
TBPline = [] # Bode Phase angle Trace line channel B - A
TAFRline = [] # Bode F reference Trace line channel A
TBFRline = [] # Bode F reference Trace line channel B
TAPRline = [] # Bode Phase reference Trace line channel A - B
TBPRline = [] # Bode Phase reference Trace line channel B - A
TBPMline = [] # Bode Frequency Math Trace
TBPRMline = [] # Bode Frequency reference Math Trace
For Further Reading:
http://docs.scipy.org/doc/numpy/reference/index.html
Return to ALICE 1.3 M1K User's Guide
Return to ALICE 2.0 M2K User's Guide