Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:tools:m1k:alice-ltc1043-analog-mux-ug [17 Apr 2021 18:33]
Doug Mercer [Be Aware when using Chop Sweep Mode]
university:tools:m1k:alice-ltc1043-analog-mux-ug [17 Apr 2021 20:23] (current)
Doug Mercer [Building the Mux]
Line 72: Line 72:
  
 There is a solder jumper, SJ1, in series with the CH-A AWG output pin between the right angle connector to the M1k and the female header. Leave this jumper open and connect the second from the top pin on the female header to digital I/O pin 0 when using the board in the Alternate Sweep configurations. To use the board in the Chop Sweep configuration,​ short the jumper. There is a solder jumper, SJ1, in series with the CH-A AWG output pin between the right angle connector to the M1k and the female header. Leave this jumper open and connect the second from the top pin on the female header to digital I/O pin 0 when using the board in the Alternate Sweep configurations. To use the board in the Chop Sweep configuration,​ short the jumper.
 +
 +{{ :​university:​tools:​m1k:​alice-ltc1043-analog-mux-fig10.png?​375 |}}
 +
 +<WRAP centeralign>​LTC1043 multiplexer PCB connected to M1k</​WRAP>​
 +
  
 =====Be Aware when using Chop Sweep Mode===== =====Be Aware when using Chop Sweep Mode=====
university/tools/m1k/alice-ltc1043-analog-mux-ug.1618677225.txt.gz · Last modified: 17 Apr 2021 18:33 by Doug Mercer