This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:tools:m1k:alice-ltc1043-analog-mux-ug [17 Apr 2021 18:33] – [Be Aware when using Chop Sweep Mode] Doug Mercer | university:tools:m1k:alice-ltc1043-analog-mux-ug [17 Apr 2021 20:23] (current) – [Building the Mux] Doug Mercer | ||
---|---|---|---|
Line 72: | Line 72: | ||
There is a solder jumper, SJ1, in series with the CH-A AWG output pin between the right angle connector to the M1k and the female header. Leave this jumper open and connect the second from the top pin on the female header to digital I/O pin 0 when using the board in the Alternate Sweep configurations. To use the board in the Chop Sweep configuration, | There is a solder jumper, SJ1, in series with the CH-A AWG output pin between the right angle connector to the M1k and the female header. Leave this jumper open and connect the second from the top pin on the female header to digital I/O pin 0 when using the board in the Alternate Sweep configurations. To use the board in the Chop Sweep configuration, | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
=====Be Aware when using Chop Sweep Mode===== | =====Be Aware when using Chop Sweep Mode===== |