This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:labs:software:precision_adc_toolbox [21 Oct 2020 22:16] – Final text, figure numbering, let's call this rev 1.0 Mark Thoren | university:labs:software:precision_adc_toolbox [19 Sep 2022 22:53] (current) – [Materials] Update python code location Mark Thoren | ||
---|---|---|---|
Line 12: | Line 12: | ||
* Raspberry Pi 4; 2G, 4G, or 8G version. (3B, 3B Plus will work, but you will want the 4 :-) ) | * Raspberry Pi 4; 2G, 4G, or 8G version. (3B, 3B Plus will work, but you will want the 4 :-) ) | ||
* 5V USB-C wall adapter for Raspberry Pi (micro USB for model 3) | * 5V USB-C wall adapter for Raspberry Pi (micro USB for model 3) | ||
- | * [[https:// | + | * [[adi>en/ |
* Electrical connection hardware (choose one): | * Electrical connection hardware (choose one): | ||
* 12x 15cm socket-to-socket jumpers such as [[https:// | * 12x 15cm socket-to-socket jumpers such as [[https:// | ||
Line 20: | Line 20: | ||
* HDMI monitor, keyboard, mouse plugged directly into Raspberry Pi | * HDMI monitor, keyboard, mouse plugged directly into Raspberry Pi | ||
* Host Windows/ | * Host Windows/ | ||
- | * [[https:// | + | * [[adi>en/ |
* 10kΩ resistors (2) | * 10kΩ resistors (2) | ||
* 10Ω resistor | * 10Ω resistor | ||
* 1kΩ resistor | * 1kΩ resistor | ||
* Breadboard or prototyping board, hookup wire | * Breadboard or prototyping board, hookup wire | ||
- | * Clone or download zip of the [[https://github.com/mthoren-adi/precision_adc_toolbox|Python | + | * Clone or download zip of the Python code for this tutorial |
+ | |||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * LTspice files: | ||
+ | </ | ||
\\ | \\ | ||
Line 243: | Line 248: | ||
==== Toolbox Item: Libm2k ==== | ==== Toolbox Item: Libm2k ==== | ||
\\ | \\ | ||
- | The signal source for the input noise mesaurement was easy - it was simply the noise inherent in the ADC itself. But it's useful to be able to send idealized test signals to the ADC to verify that it will work in the intended application, | + | The signal source for the input noise mesaurement was easy - it was simply the noise inherent in the ADC itself. But it's useful to be able to send idealized test signals to the ADC to verify that it will work in the intended application, |
\\ | \\ | ||
==== Experiment: libm2k Voice Reverser ==== | ==== Experiment: libm2k Voice Reverser ==== |