Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
university:courses:tutorials:alm-power-profiler [21 Oct 2022 15:36] – [DC Power Profiling] Doug Merceruniversity:courses:tutorials:alm-power-profiler [21 Oct 2022 16:01] (current) – [Special Power Profiler Software:] Doug Mercer
Line 79: Line 79:
 =====Special Power Profiler Software:===== =====Special Power Profiler Software:=====
  
-The ALICE desktop software can of course be used to capture the test voltage and current measurements vs time but it is not ideally suited to this application. The Data Logger tool is closer but lacks the ability to display the current or power over time. The Power Profiler tool adds this functionality.+The ALICE desktop software can of course be used to capture the test voltage and current measurements vs time but it is not ideally suited to this application. The Data Logger tool is closer but lacks the ability to display the current or power over time. The Power Profiler tool adds this functionality. Python source code can be found [[https://raw.githubusercontent.com/analogdevicesinc/alice/Version-1.3/power-profiler-1.3.pyw|here]].
  
 Once the program is running the main time trace display and controls, as shown in figure 7, should appear. Be sure that the ALM1000 is plugged into the USB port before starting the program. When first started the chart will be blank.  Once the program is running the main time trace display and controls, as shown in figure 7, should appear. Be sure that the ALM1000 is plugged into the USB port before starting the program. When first started the chart will be blank. 
university/courses/tutorials/alm-power-profiler.txt · Last modified: 21 Oct 2022 16:01 by Doug Mercer