This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:courses:engineering_discovery:lab_7 [04 Aug 2016 23:38] – Jonathan Pearson | university:courses:engineering_discovery:lab_7 [03 Jan 2018 19:45] (current) – [Observations and Conclusions] Doug Mercer | ||
---|---|---|---|
Line 65: | Line 65: | ||
* A comparator can be used to convert the continuously variable phototransistor output voltage to a binary output | * A comparator can be used to convert the continuously variable phototransistor output voltage to a binary output | ||
* A LED and phototransistor can be used to detect when an opaque object is placed between them | * A LED and phototransistor can be used to detect when an opaque object is placed between them | ||
+ | |||
+ | **Return to [[university: | ||