This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:engineering_discovery:lab_1 [03 Jan 2018 19:32] – [Observations and Conclusions] Doug Mercer | university:courses:engineering_discovery:lab_1 [21 Dec 2018 07:15] (current) – [Objective] SANTHAN KUMAR NAREDDULA | ||
---|---|---|---|
Line 4: | Line 4: | ||
==== Introduction ==== | ==== Introduction ==== | ||
- | Today’s electronic devices are made up of a wide variety of components. | + | Today’s electronic devices are made up of a wide variety of components. |
==== Objective ==== | ==== Objective ==== | ||
- | To introduce resistors, capacitors, and inductors as examples of passive components. | + | To introduce resistors, capacitors and inductors as examples of passive components. |
==== Materials and Apparatus ==== | ==== Materials and Apparatus ==== | ||
* Resistor and capacitor code handouts | * Resistor and capacitor code handouts | ||
Line 35: | Line 35: | ||
- Identify the following capacitors in the kit by using the [[university: | - Identify the following capacitors in the kit by using the [[university: | ||
- Identify the following inductors in the kit: 1.0 μH, 10 μH, 100 μH | - Identify the following inductors in the kit: 1.0 μH, 10 μH, 100 μH | ||
- | - Identify the 1N914 and 1N4001 diodes in the kit | + | - Identify the LED' |
- Identify the 2N3904 transistor in the kit | - Identify the 2N3904 transistor in the kit | ||
- | - Identify the OP484 op-amp IC in the kit | + | - Identify the OP484, |
+ | - Identify the audio jack port,micro USB port, | ||
==== Theory ==== | ==== Theory ==== | ||
The components introduced in this lab will be used in the following labs to construct circuits that increase in complexity as the labs go on. The first of the subsequent labs uses two of the passive elements – resistors and capacitors – in ways that help illustrate how these elements behave in circuits. | The components introduced in this lab will be used in the following labs to construct circuits that increase in complexity as the labs go on. The first of the subsequent labs uses two of the passive elements – resistors and capacitors – in ways that help illustrate how these elements behave in circuits. |