This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:text:glossary [28 Aug 2013 15:28] – [V] Doug Mercer | university:courses:electronics:text:glossary [05 Apr 2021 19:04] (current) – [D] Doug Mercer | ||
---|---|---|---|
Line 319: | Line 319: | ||
<WRAP indent > The process of adding impurity atoms to intrinsic (pure) silicon or germanium to improve the conductivity of the semiconductor material. </ | <WRAP indent > The process of adding impurity atoms to intrinsic (pure) silicon or germanium to improve the conductivity of the semiconductor material. </ | ||
+ | **Duty cycle** | ||
+ | <WRAP indent > Duty cycle is the fraction of one period in which a signal or system is active. Duty cycle is commonly expressed as a percentage or a ratio. A period is the time it takes for a signal to complete an on-and-off cycle. </ | ||
===== E===== | ===== E===== | ||
Line 859: | Line 860: | ||
**zener diode** | **zener diode** | ||
<WRAP indent > Semiconductor diode in which reverse breakdown voltage current causes the diode to develop a constant voltage. Used as a clamp for voltage regulation. </ | <WRAP indent > Semiconductor diode in which reverse breakdown voltage current causes the diode to develop a constant voltage. Used as a clamp for voltage regulation. </ | ||
+ | |||
+ | **Return to [[university: | ||
+ | |||
+ | **Go to Next Chapter** | ||
+ | |||
+ | **Return to [[university: | ||