Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:text:glossary [05 Sep 2013 20:03]
Doug Mercer [Z]
university:courses:electronics:text:glossary [05 Apr 2021 19:04]
Doug Mercer [D]
Line 319: Line 319:
 <WRAP indent > The process of adding impurity atoms to intrinsic (pure) silicon or germanium to improve the conductivity of the semiconductor material. </​WRAP>​ <WRAP indent > The process of adding impurity atoms to intrinsic (pure) silicon or germanium to improve the conductivity of the semiconductor material. </​WRAP>​
  
 +**Duty cycle** 
 +<WRAP indent > Duty cycle is the fraction of one period in which a signal or system is active. Duty cycle is commonly expressed as a percentage or a ratio. A period is the time it takes for a signal to complete an on-and-off cycle. </​WRAP>​
 ===== E===== ===== E=====
  
university/courses/electronics/text/glossary.txt · Last modified: 05 Apr 2021 19:04 by Doug Mercer